element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Need help identifying an early 90s PCB thru-hole transformer and a few other questions
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 20 replies
  • Answers 7 answers
  • Subscribers 34 subscribers
  • Views 4275 views
  • Users 0 members are here
Related

Need help identifying an early 90s PCB thru-hole transformer and a few other questions

chrisbc
chrisbc over 8 years ago

Hi. I need help identifying an early 90s PCB transformer. It's on an auto-idle control board from an early 90s gas-powered generator from a company that has since gone out of business. I'm not familiar with components but think I can identify all of the other components to remake another board in case of a catastrophic failure. The problem I'm having is identifying the size and type of what I think is a transformer. I've included a few pictures. It's located at the bottom of the board and has a yellow and red wire wrapped around it. The red wire comes from the generator head and goes out to a breaker to power the receptacles, and the yellow wire comes from a terminal lug next to another terminal lug which accepts the other (yellow) wire coming from the generator head.imageimageimage

And can anyone tell how big the small capacitor is that's located to the right above the transformer? I can't find any marks on it other than the temperature rating.

 

I also have to replace a 5W 82ohm resistor that blew due to a bad Schottky diode that I've found and will replace. Would it be safer to replace the blown resistor with a 12W 82ohm resistor? And can I use an aluminum encased surface mount resistor on a thru-hole PCB?

 

Any help would be appreciated!

Attachments:
image
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +4 suggested
    Hi Chris, The small capacitor is probably marked on the side that is glued down. You may have to pry it loose carefully. You can up the wattage of a resistor without any consequence except that of a larger…
  • jw0752
    jw0752 over 8 years ago in reply to chrisbc +4 suggested
    Hi Chris, If you mount a power resistor on the board make sure it is in a raised position so air is free to flow around it. This will keep it from damaging the board. You may not get the full wattage dissipation…
  • three-phase
    three-phase over 8 years ago +3 suggested
    I would agree with jw0752 that the small transformer is a current transformer measuring the load on the sockets to allow the engine speed to be controlled based upon the load the generator is supplying…
Parents
  • three-phase
    0 three-phase over 8 years ago

    I would agree with jw0752 that the small transformer is a current transformer measuring the load on the sockets to allow the engine speed to be controlled based upon the load the generator is supplying. As John as said they are usually very robust.

     

    If you do have concerns about it, they can be tested by injecting a current through the primary and measuring the output current on the secondary, depending on your circuits the output current may be converted into a voltage. If you take a few readings at different current inputs you will be able to plot the ratio, which should be consistent across the range. This of course depends on what test apparatus you have and the setup you can achieve.

     

    If you have a failure, coils can generally be rewound by dismantling them and identifying the wire size an number of turns, quite a slow painstaking job for something that small.

     

    Kind regards

     

    Donald

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • three-phase
    0 three-phase over 8 years ago

    I would agree with jw0752 that the small transformer is a current transformer measuring the load on the sockets to allow the engine speed to be controlled based upon the load the generator is supplying. As John as said they are usually very robust.

     

    If you do have concerns about it, they can be tested by injecting a current through the primary and measuring the output current on the secondary, depending on your circuits the output current may be converted into a voltage. If you take a few readings at different current inputs you will be able to plot the ratio, which should be consistent across the range. This of course depends on what test apparatus you have and the setup you can achieve.

     

    If you have a failure, coils can generally be rewound by dismantling them and identifying the wire size an number of turns, quite a slow painstaking job for something that small.

     

    Kind regards

     

    Donald

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • chrisbc
    0 chrisbc over 8 years ago in reply to three-phase

    Thanks Donald. That's definitely something I'll keep in mind for future reference.

    I've noticed that Desa had slightly revised their board design in 1998. I've found both of the 68k resistors to be toast; they are 1/4w and the newer revised board looks to have 1/2w resistors, which is what I'll replace them with. The 1k and 2k resistors are fine.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jleblanc321
    0 jleblanc321 over 7 years ago in reply to chrisbc

    Hi!

     

    I am trying to repair the same type of PCB.  I have it almost figured out, but I need to know if SC1 and SC2 are the same P/N.  My SC2 is fried, along with the resistor, so I cannot read the writing on the face of the TO-92 housing.  SC1 is a X0205NA SCR based on the writing on the TO-92 face.

     

    Thank you,

    Jay