element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 92 replies
  • Subscribers 46 subscribers
  • Views 8258 views
  • Users 0 members are here
Related

How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!

bluescreen
bluescreen over 15 years ago
Ben Heck needs your help! In the latest episode he explores different ways to build a solenoid-powered automatic can crusher. They're looking for your suggestions on different ways to build and power the can crusher. Post your suggestions here for a chance to win a Ben Heck Show t-shirt! Ten submissions will be randomly selected after Oct. 24.
 
Just post a reply to this thread with your ideas, and you'll be automatically enrolled in the t-shirt giveaway.
 
We're looking forward to your suggestions!
 
Cheers,
Sagar
  • Sign in to reply
  • Cancel

Top Replies

  • Ashen
    Ashen over 15 years ago +1
    We have built these before at my work in our spare time using old pnumatic air cylinders. 50lbs of air pressure is sufficent to crush even a large beer can. Get a cheapo compressor at lowes or use a cheap…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    This one is easy. Some college friends and I built a very effective can crusher in college to solve our large empty beer can problem. We simply used a pneumatic cylinder with a large washer attached to…
  • Viperforce30
    Viperforce30 over 15 years ago in reply to e14 Contributor +1
    I know one thing that helps when crushing a can is too slightly crease the sides of the can before hand. Maybe make the cylinder that holds the cans have a bar smack the sides before crushing the can.
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Take a two cylinder engine and elongate one cylinder and piston so that you can put a can in it, then turn over the engine once using the other cylinder. Bam one kick of the engine and you've got one flat can. Or a similar idea using a manual or electronic crank as with your design idea but using an actual engine piston so that you have the benefit of the pivoting piston head and shaft. Also the idea of having a worm screw with a direct connection to a gear with piston system is an idea worth investing into. but simple have a loading pipe end where you have the can size opening in the top with a magazine. And then having a bottom slot cut into the pipe the size of the crushed can. Walla constant feed and gravity ejection of crushed cans. This way you don't have to worry about how long it takes to crush a single can due to the high torque ratio of the worm screw.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Take a two cylinder engine and elongate one cylinder and piston so that you can put a can in it, then turn over the engine once using the other cylinder. Bam one kick of the engine and you've got one flat can. Or a similar idea using a manual or electronic crank as with your design idea but using an actual engine piston so that you have the benefit of the pivoting piston head and shaft. Also the idea of having a worm screw with a direct connection to a gear with piston system is an idea worth investing into. but simple have a loading pipe end where you have the can size opening in the top with a magazine. And then having a bottom slot cut into the pipe the size of the crushed can. Walla constant feed and gravity ejection of crushed cans. This way you don't have to worry about how long it takes to crush a single can due to the high torque ratio of the worm screw.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Comic relief....

    http://www.ebaumsworld.com/video/watch/81088486/