element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 92 replies
  • Subscribers 46 subscribers
  • Views 8258 views
  • Users 0 members are here
Related

How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!

bluescreen
bluescreen over 15 years ago
Ben Heck needs your help! In the latest episode he explores different ways to build a solenoid-powered automatic can crusher. They're looking for your suggestions on different ways to build and power the can crusher. Post your suggestions here for a chance to win a Ben Heck Show t-shirt! Ten submissions will be randomly selected after Oct. 24.
 
Just post a reply to this thread with your ideas, and you'll be automatically enrolled in the t-shirt giveaway.
 
We're looking forward to your suggestions!
 
Cheers,
Sagar
  • Sign in to reply
  • Cancel

Top Replies

  • Ashen
    Ashen over 15 years ago +1
    We have built these before at my work in our spare time using old pnumatic air cylinders. 50lbs of air pressure is sufficent to crush even a large beer can. Get a cheapo compressor at lowes or use a cheap…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    This one is easy. Some college friends and I built a very effective can crusher in college to solve our large empty beer can problem. We simply used a pneumatic cylinder with a large washer attached to…
  • Viperforce30
    Viperforce30 over 15 years ago in reply to e14 Contributor +1
    I know one thing that helps when crushing a can is too slightly crease the sides of the can before hand. Maybe make the cylinder that holds the cans have a bar smack the sides before crushing the can.
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I think that an automating the feed system will effectively negate the need for high speed crushing.

     

    I have attached a quick sketch of my idea.

     

    The system would be a fairly simple gravity fed hopper, of a type I have seen coupled with Arm-Strong can crushers. A hopper positioned above the crushing piston and would have the cans prearranged in a manner that would facilitate the crushing process.

     

    A can would fall in place before the crushing piston and prevent any further cans from falling in. This is very very much like the ammunition feed system in a original Gatling Gun. The piston would begin to crush the can, pushing it out of the way of the waiting cans. The piston itself would prevent the cans from loading until the piston has returned. Again, much like the bolt in a Gatling Gun.

     

    On the other end of the containment cylinder, a crushing bulkhead would provide the resistance necessary to crush the can. I understand this differs from Ben's design and would require that this bulkhead be firmly mounted to the super structure of the device.

     

    Once the can comes in contact with a pressure sensor, the bomb-bay style doors would open allowing the crushed can to drop out once the piston begins to retract. This would need to be on some kind of delay to prevent jamming. Once the piston retracts, the crushed can can fall into the recycle bin.

     

    The piston will then return to the original position, allowing the next can to drop into place.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I think that an automating the feed system will effectively negate the need for high speed crushing.

     

    I have attached a quick sketch of my idea.

     

    The system would be a fairly simple gravity fed hopper, of a type I have seen coupled with Arm-Strong can crushers. A hopper positioned above the crushing piston and would have the cans prearranged in a manner that would facilitate the crushing process.

     

    A can would fall in place before the crushing piston and prevent any further cans from falling in. This is very very much like the ammunition feed system in a original Gatling Gun. The piston would begin to crush the can, pushing it out of the way of the waiting cans. The piston itself would prevent the cans from loading until the piston has returned. Again, much like the bolt in a Gatling Gun.

     

    On the other end of the containment cylinder, a crushing bulkhead would provide the resistance necessary to crush the can. I understand this differs from Ben's design and would require that this bulkhead be firmly mounted to the super structure of the device.

     

    Once the can comes in contact with a pressure sensor, the bomb-bay style doors would open allowing the crushed can to drop out once the piston begins to retract. This would need to be on some kind of delay to prevent jamming. Once the piston retracts, the crushed can can fall into the recycle bin.

     

    The piston will then return to the original position, allowing the next can to drop into place.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    I had a similar idea, but I don't think you need a door to activate; the full-size can wouldn't drop through the slot for a crushed can, and the can wouldn't drop until the piston removed pressure from the can.  Gravity could do the rest.  I thought of the hopper idea, but how would we get it to automatically orient the cans so they would enter the crushing cylinder properly?