element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 92 replies
  • Subscribers 46 subscribers
  • Views 8264 views
  • Users 0 members are here
Related

How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!

bluescreen
bluescreen over 15 years ago
Ben Heck needs your help! In the latest episode he explores different ways to build a solenoid-powered automatic can crusher. They're looking for your suggestions on different ways to build and power the can crusher. Post your suggestions here for a chance to win a Ben Heck Show t-shirt! Ten submissions will be randomly selected after Oct. 24.
 
Just post a reply to this thread with your ideas, and you'll be automatically enrolled in the t-shirt giveaway.
 
We're looking forward to your suggestions!
 
Cheers,
Sagar
  • Sign in to reply
  • Cancel

Top Replies

  • Ashen
    Ashen over 15 years ago +1
    We have built these before at my work in our spare time using old pnumatic air cylinders. 50lbs of air pressure is sufficent to crush even a large beer can. Get a cheapo compressor at lowes or use a cheap…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    This one is easy. Some college friends and I built a very effective can crusher in college to solve our large empty beer can problem. We simply used a pneumatic cylinder with a large washer attached to…
  • Viperforce30
    Viperforce30 over 15 years ago in reply to e14 Contributor +1
    I know one thing that helps when crushing a can is too slightly crease the sides of the can before hand. Maybe make the cylinder that holds the cans have a bar smack the sides before crushing the can.
Parents
  • jnissen
    0 jnissen over 15 years ago

    Pneumatic cylinders are great for something like this. The electromagnetic ram can work but it really needs to have a tight tolerance betwwen the plunger and the coil. Better yet If the coil is seperated into many segments and the plunger is actually a rare earth magnet then you could control the series of coils to rapidly accelerate the plunger/magnet. The same concept is used in rails guns. The control is not easy as you have to switch the high currents very quickly and in a manner that will sequence the electromagnetic force so that it will properly accelerate the projectile. Some feedback sensing to help in the control would be required to do it effectivly. Yeah a rail gun can crusher would be a significant step up in cool.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jnissen
    0 jnissen over 15 years ago

    Pneumatic cylinders are great for something like this. The electromagnetic ram can work but it really needs to have a tight tolerance betwwen the plunger and the coil. Better yet If the coil is seperated into many segments and the plunger is actually a rare earth magnet then you could control the series of coils to rapidly accelerate the plunger/magnet. The same concept is used in rails guns. The control is not easy as you have to switch the high currents very quickly and in a manner that will sequence the electromagnetic force so that it will properly accelerate the projectile. Some feedback sensing to help in the control would be required to do it effectivly. Yeah a rail gun can crusher would be a significant step up in cool.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to jnissen

    A method of crushing cans while also stimulating people to get excercise and relieve stress woudl be to have a hopper attached to a modified "Bash the gopher" machine.

     

    Once the machine had collected enough cans for a game it would start flashing and playing music.

     

    Everyone would cheer and haul themselves off the couch to lumber over to the machine and then they would discuss who was going first, stimulating healthy conversation amongst the family members.

     

    Once Dad had decided he would go first , he would take the mallet in his hand and the machine would pop cans randomly out of the holes on the top of the playing surface and he would bash away as the family cheer and offer advice.

     

    Each member of the family would take turns until all the cans were flat and they would all smile at each other and offer hearty congratulations or mock teasing as they returned to their TV, tired but happy.

     

    TRM