element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 92 replies
  • Subscribers 46 subscribers
  • Views 8264 views
  • Users 0 members are here
Related

How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!

bluescreen
bluescreen over 15 years ago
Ben Heck needs your help! In the latest episode he explores different ways to build a solenoid-powered automatic can crusher. They're looking for your suggestions on different ways to build and power the can crusher. Post your suggestions here for a chance to win a Ben Heck Show t-shirt! Ten submissions will be randomly selected after Oct. 24.
 
Just post a reply to this thread with your ideas, and you'll be automatically enrolled in the t-shirt giveaway.
 
We're looking forward to your suggestions!
 
Cheers,
Sagar
  • Sign in to reply
  • Cancel

Top Replies

  • Ashen
    Ashen over 15 years ago +1
    We have built these before at my work in our spare time using old pnumatic air cylinders. 50lbs of air pressure is sufficent to crush even a large beer can. Get a cheapo compressor at lowes or use a cheap…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    This one is easy. Some college friends and I built a very effective can crusher in college to solve our large empty beer can problem. We simply used a pneumatic cylinder with a large washer attached to…
  • Viperforce30
    Viperforce30 over 15 years ago in reply to e14 Contributor +1
    I know one thing that helps when crushing a can is too slightly crease the sides of the can before hand. Maybe make the cylinder that holds the cans have a bar smack the sides before crushing the can.
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I would use a simple shift screw attached to a single stage gear reduction. It would be slower, but far more effective then attaching the motor directly to the mechanism.

     

    The screw could be attached centrally to two platforms. Two shafts acting as stablizer bars on each side should keep the two platforms in place while the screw extends and contracts the upper platform.

     

    With a screw and single stage gear this would allow the motor and other assortments to be attached on the back of the unit for a very clean and minimal design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I would use a simple shift screw attached to a single stage gear reduction. It would be slower, but far more effective then attaching the motor directly to the mechanism.

     

    The screw could be attached centrally to two platforms. Two shafts acting as stablizer bars on each side should keep the two platforms in place while the screw extends and contracts the upper platform.

     

    With a screw and single stage gear this would allow the motor and other assortments to be attached on the back of the unit for a very clean and minimal design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Ben should use the very old ding don bell structure to quickly crush the CAN, All it need is an electromagnet and movable piston

    within a fraction the CAN is crushed , The amount of power needed will also be small as comapre to motor ideas the needed specs are

    all suffice by this idea

    1: force                 should be great and momentarly

    2:Power               Only at the actuating the electromagnet

    3:Standby            Nil

    4:Counitng           shouild be easy enough

    5:Batteries          can be used with capaciotrs banks ,to store the required energy

     

    Thanks

    Manish jain