element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 92 replies
  • Subscribers 46 subscribers
  • Views 8286 views
  • Users 0 members are here
Related

How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!

bluescreen
bluescreen over 15 years ago
Ben Heck needs your help! In the latest episode he explores different ways to build a solenoid-powered automatic can crusher. They're looking for your suggestions on different ways to build and power the can crusher. Post your suggestions here for a chance to win a Ben Heck Show t-shirt! Ten submissions will be randomly selected after Oct. 24.
 
Just post a reply to this thread with your ideas, and you'll be automatically enrolled in the t-shirt giveaway.
 
We're looking forward to your suggestions!
 
Cheers,
Sagar
  • Sign in to reply
  • Cancel

Top Replies

  • Ashen
    Ashen over 15 years ago +1
    We have built these before at my work in our spare time using old pnumatic air cylinders. 50lbs of air pressure is sufficent to crush even a large beer can. Get a cheapo compressor at lowes or use a cheap…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    This one is easy. Some college friends and I built a very effective can crusher in college to solve our large empty beer can problem. We simply used a pneumatic cylinder with a large washer attached to…
  • Viperforce30
    Viperforce30 over 15 years ago in reply to e14 Contributor +1
    I know one thing that helps when crushing a can is too slightly crease the sides of the can before hand. Maybe make the cylinder that holds the cans have a bar smack the sides before crushing the can.
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I posted a reply on the episode page with some ideasnot knowing this discussion was going on, perhaps some admin could post a message with a link to this discussion; to sum it up, lets not completly reinvent the wheel, but put some nice rims on it, I think the most efficient thing would be to start with an off the shelf can crusher and use the  wormgear assembly out of an adjustable car seat to draw it closed, this would be a good source of linear movement, so  you'd need to make a U- shaped bracket that pivots on the handle of the crusher, as well as pivoting on the carriage portion that moves along the leadscrew, it would need to be mounted so the lead screw ended before the bottom of the crusher, so you can still pu the can in it. you would need limit switches and some relays that would work as a reversing one-shot  motor starter. this could be accomplished with acouple relays, a limit switch to break the latch on the forward relay and strart the reversed relays so it automatically opens back up, then you'd need a limit switch to stop it when it's once again in the open position. then of course you could implemant some sort of start swith that is trigger when a can is placed in the crusher. otherwise you'd start button to start the whole process. I'll draw up a simple schematic with crude illustration and post it when I have time.

    Deep C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    I posted a reply on the episode page with some ideasnot knowing this discussion was going on, perhaps some admin could post a message with a link to this discussion; to sum it up, lets not completly reinvent the wheel, but put some nice rims on it, I think the most efficient thing would be to start with an off the shelf can crusher and use the  wormgear assembly out of an adjustable car seat to draw it closed, this would be a good source of linear movement, so  you'd need to make a U- shaped bracket that pivots on the handle of the crusher, as well as pivoting on the carriage portion that moves along the leadscrew, it would need to be mounted so the lead screw ended before the bottom of the crusher, so you can still pu the can in it. you would need limit switches and some relays that would work as a reversing one-shot  motor starter. this could be accomplished with acouple relays, a limit switch to break the latch on the forward relay and strart the reversed relays so it automatically opens back up, then you'd need a limit switch to stop it when it's once again in the open position. then of course you could implemant some sort of start swith that is trigger when a can is placed in the crusher. otherwise you'd start button to start the whole process. I'll draw up a simple schematic with crude illustration and post it when I have time.

    Deep C