element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 92 replies
  • Subscribers 46 subscribers
  • Views 8296 views
  • Users 0 members are here
Related

How should Ben continue building his automatic can crusher? Post your idea + you might get a free Ben Heck t-shirt!

bluescreen
bluescreen over 15 years ago
Ben Heck needs your help! In the latest episode he explores different ways to build a solenoid-powered automatic can crusher. They're looking for your suggestions on different ways to build and power the can crusher. Post your suggestions here for a chance to win a Ben Heck Show t-shirt! Ten submissions will be randomly selected after Oct. 24.
 
Just post a reply to this thread with your ideas, and you'll be automatically enrolled in the t-shirt giveaway.
 
We're looking forward to your suggestions!
 
Cheers,
Sagar
  • Sign in to reply
  • Cancel

Top Replies

  • Ashen
    Ashen over 15 years ago +1
    We have built these before at my work in our spare time using old pnumatic air cylinders. 50lbs of air pressure is sufficent to crush even a large beer can. Get a cheapo compressor at lowes or use a cheap…
  • e14 Contributor
    e14 Contributor over 15 years ago +1
    This one is easy. Some college friends and I built a very effective can crusher in college to solve our large empty beer can problem. We simply used a pneumatic cylinder with a large washer attached to…
  • Viperforce30
    Viperforce30 over 15 years ago in reply to e14 Contributor +1
    I know one thing that helps when crushing a can is too slightly crease the sides of the can before hand. Maybe make the cylinder that holds the cans have a bar smack the sides before crushing the can.
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Wow, I came into this late so I'm guessing the can crusher project was  scrapped. But, just to throw in my 2 cents, I would suggest a windshield  wiper motor and an Hbridge high power servo board to actuate and  control the can crusher. Car windshield wiper motors are pre built with a  worm gear, can operate at 5-12 Vcc, and have (usually) 2 or more  connectors to operate at different speeds, plus they have MONSTER  torque! This can be made into a hi power servo by linking the motor to  an Hbridge circuit from Parallax.com which is around 15 bucks. A wiper  motor is about the same price (15 bucks) new, but pulled from grandmas  car (she refuses to drive in the rain anyways, right?) you can get it  for free. The challenge would be mounting a 5V POT to the rotation shaft  of the motor for position feedback to whatever servo controller board  you choose. You could even use a remote control model airplane  controller to make the servo work, or you could ditch the whole servo  idea altogether and take advantage of the parking feature that SOME  windshield wiper motors already come with. This means that the wiper  motor shaft will return to the original position after one rotation of  the shaft and would allow the motor to be actuated with a simple relay.  Just a thought.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Wow, I came into this late so I'm guessing the can crusher project was  scrapped. But, just to throw in my 2 cents, I would suggest a windshield  wiper motor and an Hbridge high power servo board to actuate and  control the can crusher. Car windshield wiper motors are pre built with a  worm gear, can operate at 5-12 Vcc, and have (usually) 2 or more  connectors to operate at different speeds, plus they have MONSTER  torque! This can be made into a hi power servo by linking the motor to  an Hbridge circuit from Parallax.com which is around 15 bucks. A wiper  motor is about the same price (15 bucks) new, but pulled from grandmas  car (she refuses to drive in the rain anyways, right?) you can get it  for free. The challenge would be mounting a 5V POT to the rotation shaft  of the motor for position feedback to whatever servo controller board  you choose. You could even use a remote control model airplane  controller to make the servo work, or you could ditch the whole servo  idea altogether and take advantage of the parking feature that SOME  windshield wiper motors already come with. This means that the wiper  motor shaft will return to the original position after one rotation of  the shaft and would allow the motor to be actuated with a simple relay.  Just a thought.