• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 360 slim reliability
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 29 subscribers
  • Views 513 views
  • Users 0 members are here
  • 360
  • slim
Related

360 slim reliability

e14 Contributor
e14 Contributor over 15 years ago
Ben,
Can you comment on how reliable you think the 360 slim is compared to older models as far as reliability?  You should be very qualified to answer that.
I purchased the original 360 - it ringed - then purchased the original elite - it ringed - now I have the slim.  I can't imagine if I were a serious gamer.Ben,
Can you comment on how reliable you think the 360 slim is compared to older models as far as reliability?  You should be very qualified to answer that.
I purchased the original 360 - it ringed - then purchased the original elite - it ringed - now I have the slim.  I can't imagine if I were a serious gamer.
Ben,
Can you comment on how reliable you think the 360 slim is compared to the older models?  You should be very qualified to answer that.
I purchased the original 360 - it ringed - then purchased the original elite - it ringed - now I have the slim.  I can't imagine if I were a serious gamer.
thanks for the great show,
-Scott
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    The original design of the Xbox 360 was plagued by several design flaws. They did come out with several motherboard revisions and a few minor case revisions. However the majority of the issues were never addressed in the original design. When you take the plastic case off of the Xbox 360, you are greeted by a interior metal case. The motherboard is held to this case with a few different screws. This is where the  main flaw of the Xbox 360 lies. The way that the case is designed allows the motherboard to bend and flex. This can be especially problematic in humid areas where the moisture in the air can aid the motherboard in bending in the middle. The interior metal casing does not provide enough support to keep the motherboard from bending. When the motherboard bends, it puts stress on the solder joints beneath the CPU chip and the GPU chip that are located in the middle of the motherboard. Over time, these solder balls will begin to separate from the chip and then you get the red ring. There are actually over 50 different errors that are represented by the red ring. The main cause for all of them is the same, but it can vary based on the chip. There is also a phenomenom called "tin whiskers" that has been found in the Xbox 360. The solder that Microsoft used when they built the console contains a high percentage of tin. Over time, tin can grow little crystals that are known as "tin whiskers". These crystals can grow at a rate of 1 mm per year and over time can actually bridge components.

     

    So to answer your question, the new Xbox 360 slim has a completely different motherboard and chipset. They have combined the GPU and CPU onto one chip and added an actual fan on top of the heatsink. The casing seems to provide better support, so the main cause of the Red Ring appears to have been eliminated. However, other causes such as "Tin whiskers" may still appear. It does not appear that the new 360 has nearly the failure rate of the older models.

     

    I've gone through hundreds of Xbox 360's and I've seen pretty much every issue that can possibly come up. None of it is enough to keep me from enjoying my console. Hope that this answers your question!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    The original design of the Xbox 360 was plagued by several design flaws. They did come out with several motherboard revisions and a few minor case revisions. However the majority of the issues were never addressed in the original design. When you take the plastic case off of the Xbox 360, you are greeted by a interior metal case. The motherboard is held to this case with a few different screws. This is where the  main flaw of the Xbox 360 lies. The way that the case is designed allows the motherboard to bend and flex. This can be especially problematic in humid areas where the moisture in the air can aid the motherboard in bending in the middle. The interior metal casing does not provide enough support to keep the motherboard from bending. When the motherboard bends, it puts stress on the solder joints beneath the CPU chip and the GPU chip that are located in the middle of the motherboard. Over time, these solder balls will begin to separate from the chip and then you get the red ring. There are actually over 50 different errors that are represented by the red ring. The main cause for all of them is the same, but it can vary based on the chip. There is also a phenomenom called "tin whiskers" that has been found in the Xbox 360. The solder that Microsoft used when they built the console contains a high percentage of tin. Over time, tin can grow little crystals that are known as "tin whiskers". These crystals can grow at a rate of 1 mm per year and over time can actually bridge components.

     

    So to answer your question, the new Xbox 360 slim has a completely different motherboard and chipset. They have combined the GPU and CPU onto one chip and added an actual fan on top of the heatsink. The casing seems to provide better support, so the main cause of the Red Ring appears to have been eliminated. However, other causes such as "Tin whiskers" may still appear. It does not appear that the new 360 has nearly the failure rate of the older models.

     

    I've gone through hundreds of Xbox 360's and I've seen pretty much every issue that can possibly come up. None of it is enough to keep me from enjoying my console. Hope that this answers your question!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    thanks for the great response!