element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Embed an arduino
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 31 subscribers
  • Views 835 views
  • Users 0 members are here
  • ask_a_question
  • ben_heck
  • arduino
Related

Embed an arduino

e14 Contributor
e14 Contributor over 14 years ago

Hi ben!

 

I am Midas from Belgium and I love your show!

I am thirteen years old and I love working with the arduino uno.

I have just a question about the arduino.

In several shows you talked about to "embedd" an arduino.

I have done this a few times with a crystal and 2 22 pF capacitors.

But in your episode abou the Xbox coin reward system I didn't see any capacitors.

Are these capacitors REALLY needed or can you leave them away?

 

Thank you for reading my question, I hope to hear from you soon.

  • Sign in to reply
  • Cancel
Parents
  • colecago
    0 colecago over 14 years ago

    If you are using a crystal, you really should use those caps.  From an atmel datasheet

     

    When using resonators with the AtmelRegisteredAVRRegistered, it is necessary to apply (external)

    capacitors according to the requirements of the facilitated resonator. A parallel

    resonator will not be able to oscillate stable if the capacitive load applied is

    insufficient. If the capacitive load is too high the oscillation may have problems

    starting due to drive level dependency of the load. The trick is therefore to find an

    appropriate value for the capacitive load. The value to look for in the data sheet of the

    crystal is CL, the recommended capacitive load of the resonator (viewed from the

    terminals of the resonator). The capacitive load, CL, of the oscillator circuit, including

    stray capacitances and the capacitances of the XTAL pins of the AVR can be

    determined empirically or it can be estimated by Equation 5-1.

     

    5.3 Recommended capacitor values

    The recommendations here will work well in most applications, but there is no way to

    provide general values for the external capacitors that can be guaranteed to work with

    all resonators.

    When using the clock option “ext. crystal oscillator”, crystals with a nominal frequency

    from 400kHz and up can be used. For these standard “high” frequency crystals the

    recommended capacitor value is in the range 22-33pF.

     

    Many AVR's include an onboard internal oscillator, usually 8Mhz, those can be used and you won't need a crystal at all.  Just make sure to set your fuse bits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • colecago
    0 colecago over 14 years ago

    If you are using a crystal, you really should use those caps.  From an atmel datasheet

     

    When using resonators with the AtmelRegisteredAVRRegistered, it is necessary to apply (external)

    capacitors according to the requirements of the facilitated resonator. A parallel

    resonator will not be able to oscillate stable if the capacitive load applied is

    insufficient. If the capacitive load is too high the oscillation may have problems

    starting due to drive level dependency of the load. The trick is therefore to find an

    appropriate value for the capacitive load. The value to look for in the data sheet of the

    crystal is CL, the recommended capacitive load of the resonator (viewed from the

    terminals of the resonator). The capacitive load, CL, of the oscillator circuit, including

    stray capacitances and the capacitances of the XTAL pins of the AVR can be

    determined empirically or it can be estimated by Equation 5-1.

     

    5.3 Recommended capacitor values

    The recommendations here will work well in most applications, but there is no way to

    provide general values for the external capacitors that can be guaranteed to work with

    all resonators.

    When using the clock option “ext. crystal oscillator”, crystals with a nominal frequency

    from 400kHz and up can be used. For these standard “high” frequency crystals the

    recommended capacitor value is in the range 22-33pF.

     

    Many AVR's include an onboard internal oscillator, usually 8Mhz, those can be used and you won't need a crystal at all.  Just make sure to set your fuse bits.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer