• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 2 operating systems in 1?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 34 subscribers
  • Views 1138 views
  • Users 0 members are here
  • apple
  • systems
  • windows
  • system_hardware
  • idea
  • desktop
  • operating
Related

2 operating systems in 1?

e14 Contributor
e14 Contributor over 13 years ago

I was wondering how cool it be if it is possible for a desktop computer to be capable to have Microsofts Windows 7 and Apple IOS snow leopard or higher.Just throwing this idea out there but it might have been done already. image

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to RadioFreeRO +1
    yes it has been done many times on the internet. No its not illlegal unless you use a cracked version of either Windows or IOS and then dual boot system is not illegal only the cracked version of the software…
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    You can do this but I suggest you do a little research because it matters which OS is installed first.

     

    I have a dual boot Linux/ Windows XP  Dell inspiron 1525. I found the info I needed on the internet. I did this because I was starting my Linux Admin Class at ITT Tech and was given the same warning about researching it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jds123
    0 jds123 over 13 years ago in reply to e14 Contributor

    The main issue is the fact that windows always rewrites the MBR. It may be easier to just use VirtualBox which is a free emulator, which will effectivly allow you to run an OS inside of another OS. It would most likely be easiest to make 3 partitions and use Linux Windows and Mac installing Linux last as it will write the MBR with GRUB which can autodetect the other OSs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jds123
    0 jds123 over 13 years ago in reply to e14 Contributor

    The main issue is the fact that windows always rewrites the MBR. It may be easier to just use VirtualBox which is a free emulator, which will effectivly allow you to run an OS inside of another OS. It would most likely be easiest to make 3 partitions and use Linux Windows and Mac installing Linux last as it will write the MBR with GRUB which can autodetect the other OSs.