element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Idea & Brain storming "adjustable size CNC" 1'x1' to 3'x3'
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 31 subscribers
  • Views 834 views
  • Users 0 members are here
  • adjustable
  • cnc_machine
Related

Idea & Brain storming "adjustable size CNC" 1'x1' to 3'x3'

e14 Contributor
e14 Contributor over 13 years ago

I know I'm shooting for the moon here, but here is the background.

I live in an apartment, and space is tight. I hope to move into a home a couple of years from now after if finish school.

I am curious if it is possible to make a CNC that can be added too to make it work for a larger area.

For now I would only like to have a CNC for about 1'x1' area, but I think it would be cool to have a grid system that would allow you to add to it without to much effort.

So for starters the cnc would run accross block "1", and then add "A" so it would be 1'x2', and then add "B" and "2" so it would be a 2x2 grid.

I realize that the movement of the CNC would have to be based on chains or gear belts so you could add to it.

Any ideas on how to make this possible.

image

image is a google sketchup file that is attached.

Attachments:
adjustableCNC.skp.zip
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I think it would be better to make it as wide as you will want it later and design it so you could make it longer in the future. This would solve the problem of the gantry not spanning the entire table. In other words start with 3'x1' instead of 1'x1'.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I think it would be better to make it as wide as you will want it later and design it so you could make it longer in the future. This would solve the problem of the gantry not spanning the entire table. In other words start with 3'x1' instead of 1'x1'.