element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Question about Arduino embedding on circuit board.
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 33 subscribers
  • Views 1126 views
  • Users 0 members are here
Related

Question about Arduino embedding on circuit board.

e14 Contributor
e14 Contributor over 13 years ago

Hi, I built a circuit using an lcd and temp sensor using the Arduino. It worked on the breadboard, but when I wired everything up to a perf board with new 328 chip (it had bootloader already on it, and I programmed it by inserting it into the dip socket of UNO), it didn't work. I triple and quadruple checked all of the connections. I am using an external 16 MHz crystal and two .1uF caps at the crystal. Can these capacitor values keep the circuit from running. Are they necessary?

 

Thanks,

Kevin

  • Sign in to reply
  • Cancel

Top Replies

  • colecago
    colecago over 13 years ago +1
    Yeah, those are way high. I think we used 18-22pF on our AVR designs. Here is a document from Atmel that talks a bit about crystal cap selection and other AVR recommendations. http://www.atmel.com/images…
  • shabaz
    0 shabaz over 13 years ago

    There is a simple formula for calculating the capacitor value, depending on your specific crystal parameter (CL), but it's late and I'm rather tired to look it up : ) Anyway, 0.1uF is definitely not good. Replace those two caps with something like 22pF and you'll be fine. That is much closer to the ballpark that you should be using (i.e. ballpark is almost 5000 times lower value than your current value of 0.1uF), and is then virtually guaranteed to work with your 16MHz xtal. And yes, they are absolutely necessary : )

    Don't forget a small cap (10nF or 100nF - i.e. 0.1uF) across the power rails very very close to your microcontroller too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Blacksheep32
    0 Blacksheep32 over 13 years ago

    Any chance you could post up your circuit?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 13 years ago

    Yeah, those are way high.  I think we used 18-22pF on our AVR designs.

     

    Here is a document from Atmel that talks a bit about crystal cap selection and other AVR recommendations.

     

    http://www.atmel.com/images/doc2521.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to Blacksheep32

    Hi, the circuit has physical Atmega328 pins 7, 20, 21 to 5v.  Pins 8 and 22 to ground. Xtal to pins 9 and 10 with .1uF caps. The RGB LCD is going to digital pins D3, and D5 thru D12 as well as appropriate vcc and ground and pot. The circuit worked when breadboarded along with the UNO. I have temp sensor on pin A0. Also reset pin is going to 5v thru 10K resistor

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to e14 Contributor

    Perhaps one board was configured to use the internal oscillator. If it is desired to use an external crystal, the 0.1uF capacitors need to be replaced with something in the region of 22pF. If it still doesn't work then it can be investigated further, but definitely the external crystal does need a far lower value. Atmel devices can often be configured to use an internal oscillator, or an external crystal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • benheck
    0 benheck over 13 years ago

    When in doubt, copy it off from the Arduino schematic!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Thanks everybody. I changed out the caps for 22pF caps. Now it works! image

     

    Now, if I can keep the TMP36 from fluctuating all over the place. It worked fine when using UNO, but jumps around sometimes as much as 20F on my embedded circuit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I just added two caps to the circuit to filter out noise, and now the temp readout is great! image