• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum iPod Speaker Dock Idea
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 33 subscribers
  • Views 1121 views
  • Users 0 members are here
  • ipod
  • help
  • hack
  • mp3_player_speaker_docks
  • hardware
  • dock
  • build_challenge
  • idea
  • viewer_challenge
  • ben_heck
Related

iPod Speaker Dock Idea

e14 Contributor
e14 Contributor over 13 years ago

I have some speakers I scrapped from a broken LCD TV, and I thought it would be a cool idea to make an iPod dock out of them. I also have a NETduino that i want to implement into this project somehow.

My main problem is the circuitry.

1.) I dont know how to amplify the sound/ what i should use to amplify it

2.) I need to be able to charge the iPod

3.) I want it to get sound from the iPod's dock connector

What i know:

the speakers have 7 ohms of resistance

Any help with this project will be greatly apprecieated

  • Sign in to reply
  • Cancel
  • colecago
    0 colecago over 13 years ago

    You wouldn't need the Netduino at all.  For the amplifier there are many options, you can pick up an audio amp and follow the guidlines in the data sheet

    http://www.newark.com/texas-instruments/lm386m-1-nopb/ic-audio-pwr-amp-class-ab-325mw/dp/41K5099

     

    or if you aren't comfortable with electronics, you can buy a kit

    https://www.sparkfun.com/products/9612

     

    for both 2 and 3 you need an ipod breakout

    https://www.sparkfun.com/products/8295

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to colecago

    Thanks almost exactly what i need, but is this variable? (the amp)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to colecago

    One more question, What could i use to Play/fast forward/skip songs?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 13 years ago in reply to e14 Contributor

    That amp has two pots on it to change the left/right channel volume.

     

    Apparently for remote controle, you can use serial commands, so you might have a use for your netduino after all

    http://www.adriangame.co.uk/ipod-acc-pro.html

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to colecago

    I looked at the schematic for the IC and it has only 1 channel, but has two pot ports should i use two and wire the pot to all four ports using a common lead?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colecago
    0 colecago over 13 years ago in reply to e14 Contributor

    Yeah, not the best IC for stereo sound I think.  Try this one

    http://www.newark.com/texas-instruments/tpa122d/amp-stereo-audio-150mw-smd-soic8/dp/26M4256

     

    -note, this one might be a bit small for your speakers.  You might have better luck with that kit for higher power.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • benheck
    0 benheck over 13 years ago

    If it's the old iPod dock (pre-Lighting) the pinout is readily available.

     

    I believe adapters, docks, etc control the iPod with serial commands (there's an RX TX on that dock)

     

    Here's a good, easy to use audio amp http://www.newark.com/texas-instruments/tpa6021a4n/ic-audio-power-amp-class-ab-2w/dp/43K4150?in_merch=Popular%20Products

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jds123
    0 jds123 over 13 years ago

    Just make a simple amplifier circuit, and just use a pinout to figure out how to connect it use this http://pinouts.ru/PortableDevices/ipod_pinout.shtml for the older connectors for the new one use the pinout on this webpage http://en.wikipedia.org/wiki/Lightning_%28connector%29 this webpage will help you build a amplifier http://www.circuitstoday.com/category/amplifier-circuits

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago

    Here is some sample C code to play and skip right/left with the old (pre-lightening) dock connector. I have tested this on the original

    iPod touch. It uses the ATmega64, but should be easy to adapt for any processor.

    To use it, call ipod_uart_init() at the start of your program, and then use the ipod_tx_cmd() command whenever you wish to

    control the iPod, e.g. ipod_tx_cmd(PLAY2) etc..

    The '2' is not important, it just means it is a so-called 'type-2' command (the iPod understands some simpler Type-1 commands too, which

    I did not implement.

     

    The instructions are in an array which could be extended for other commands if desired.

     


    // Port E

    // Ipod Rx/Tx pins: (also used as programming port MOSI/MISO)

    #define IPOD_RX 0x01

    #define IPOD_TX 0x02

     

    // ***************** COMMANDS *******************

    #define PLAY2 0

    #define SKIPR2 1

    #define SKIPL2 2

    #define REL2 3


    const unsigned char cmd_arr[]={

      /* mode 2 commands */

      /* play command */

      0x00, 0x00, 0x01,

      /* skip right */

      0x00, 0x08,

      /* skip left */

      0x00, 0x10,

      /* button release */

      0x00, 0x00

    };


    const unsigned int idx_arr[]={

      /* play */

      0,

      /* skip right */

      3,

      /* skip left */

      5,

      /* button release */

      7,

      /* terminate the array */

      9

    };


    // ipod interface (UART0)

    void ipod_uart_init(void)

    {

      // At 14.7Mhz, UBRR0 set to 47 gives 19200baud

      UBRR0H = 0;

      UBRR0L = 47;

      /* Enable receiver and transmitter */

      //UCSR0B = (1<<RXEN0)|(1<<TXEN0);

      UCSR0B = (1<<TXEN0);

      /* Set frame format: 8data, N, 1stop bit */

      UCSR0C = 0x06;

    }


    // This will transmit a single byte across the ipod interface

    void ipod_tx_byte( unsigned char data )

    {

    /* Wait for empty transmit buffer */

    while ( !( UCSR0A & (1<<UDRE0)) )

    ;

    /* Put data into buffer, sends the data */

    UDR0 = data;

    }



    // This will calculate the checksum and transmit all bytes

    void ipod_tx_bytes(unsigned char mode, unsigned char* arr, unsigned char length)

    {

      unsigned int tot;

      unsigned char j;

      unsigned int check;

      unsigned char i;


      tot=length+1+mode;

      for (j=0; j<length; j++)

      {

        tot=tot+arr[j];

      }

      check=0x100-(tot & 0xff);



      ipod_tx_byte(0xff);

      ipod_tx_byte(0x55);

      ipod_tx_byte(length+1);

      ipod_tx_byte(mode);

      for (i=0; i< length; i++)

      {

        ipod_tx_byte(arr[i]);

      }

      ipod_tx_byte((unsigned char)check);

    }


    // This will play a command from the array

    void ipod_tx_cmd(unsigned char cmd)

    {

      int i;

      unsigned int index;

      unsigned char length;


      switch (cmd)

      {

        // Mode 2 commands

        case PLAY2:

        case SKIPR2:

        case SKIPL2:

          index=idx_arr[cmd];

          length=(unsigned char) (idx_arr[cmd+1] - idx_arr[cmd]);

          // transmit these commands a few times in case the ipod misses it

          // (will this ever happen?)

          for (i=0; i<3; i++)

          {

            ipod_tx_bytes(2, (unsigned char*)&cmd_arr[index], length);

          }

          // since it was a mode 2 command, now execute 'button release'

          for (i=0; i<3; i++)

          {

            ipod_tx_bytes(2, (unsigned char*)&cmd_arr[idx_arr[REL2]], idx_arr[REL2 + 1] - idx_arr[REL2] );

          }

          break;

      default:

          break;

      }