• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Viewer Challange: Magnetic mouse/joystick base for games like Battlefield 3
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 32 subscribers
  • Views 694 views
  • Users 0 members are here
  • build_challenge
  • challenge
  • Controllers
  • ben_heck
Related

Viewer Challange: Magnetic mouse/joystick base for games like Battlefield 3

e14 Contributor
e14 Contributor over 13 years ago

Ok, I was watching old episodes of Prototype This! on Netflix and an idea sprang up into my head.

 

A mouse that uses a magnetic sensor instead of a light, and the base can double as a joystick for hopping in and out of vehicles, or playing flight sims.

 

I know of a couple difficulties, 1 would be button presses, the other would be a way to keep the joystick from sliding over the surface.

 

Maybe have it tethered to the base when you switch the mouse out, have a small bay of extra buttons and toggles for various commands that can be programmed within windows?

 

I have nearly no experiance with electronics, but I think that same bug that got you has gotten me, this would be an interesting idea that would benifit many PC gamers.

 

Thanks in advance.

  • Sign in to reply
  • Cancel
Parents
  • colecago
    0 colecago over 13 years ago

    I don't think I understand.  The base is like a magnetic mousepad and the mouse uses magnetic sensors to track across it, and joystick, is this a joystick that slides across the base like the mouse, but is joystick shaped?  Or is it a standard joystick that somehow connects to the magnetic mousepad and doesn't really use the pad?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to colecago

    Think about it like this.

     

    There is a base, the size of a standard mouse pad, possibly longer and a little wider. Below the pad is the magnetic sensor, the mouse is the magnet. Additionally, there are connections around the mousepad where a joystick can be set over the sensor, more or less making it a regular joystick.

     

    Im kind of envisioning this as a modular device, where you can replace the "Mouse" with other things, like maybe a small steering wheel. At the top is another modular spot, which can house more buttons, or a cradle for a iphone/ipad tablet...thing. I have a Kindle Fire, so it would be interesting to have a mount where it can sit in landscape mode and I can, say, put up a digital map of an area, or use a free, open source program like touchbuddy to send commands to my pc via lan.

     

    I actually drew a picture, but my scanner is being persnickity because were out of ink...but...it "could" be an interesting idea. Ill play with google sketch-up or something to give a 3d rendering of my idea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to colecago

    Think about it like this.

     

    There is a base, the size of a standard mouse pad, possibly longer and a little wider. Below the pad is the magnetic sensor, the mouse is the magnet. Additionally, there are connections around the mousepad where a joystick can be set over the sensor, more or less making it a regular joystick.

     

    Im kind of envisioning this as a modular device, where you can replace the "Mouse" with other things, like maybe a small steering wheel. At the top is another modular spot, which can house more buttons, or a cradle for a iphone/ipad tablet...thing. I have a Kindle Fire, so it would be interesting to have a mount where it can sit in landscape mode and I can, say, put up a digital map of an area, or use a free, open source program like touchbuddy to send commands to my pc via lan.

     

    I actually drew a picture, but my scanner is being persnickity because were out of ink...but...it "could" be an interesting idea. Ill play with google sketch-up or something to give a 3d rendering of my idea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    lets try this...since my scanner is a PITA image