element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Is it possible for a copy of Windows to run on a Raspberry Pi?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 22 replies
  • Subscribers 33 subscribers
  • Views 3608 views
  • Users 0 members are here
  • viewer
  • hack
  • portable
  • build
  • episode
  • build_challenge
  • idea
  • viewer_challenge
  • challenge
  • ben_heck
  • heck
  • ben
  • show_idea
Related

Is it possible for a copy of Windows to run on a Raspberry Pi?

e14 Contributor
e14 Contributor over 13 years ago

Hello i was wondering if it was possible to run either windows 8 or windows xp on a Raspberry Pi model B 512mb.

 

ever since i bought my Raspberry Pi i was always thinking of if my thought would be possible. Being a raspberry Pi it does not have the function to boot off a memory stick to install a copy of windows therefore that stopped my train of thought.

 

please someone will you be able to help me with my problem and either do a well documented walkthrough on a blog or would someone be able to make a video dissussing the topic and how to acheive this... thank you lloydpheasant.

  • Sign in to reply
  • Cancel

Top Replies

  • SGarciaV
    SGarciaV over 13 years ago +1
    I agree with Coder27. Since Raspberry Pi runs Linuz the question could changed to "Can Windows xp/8 run on Linux?". Surprisingly, the answer to this yes, but with certain reservations. The hardware that…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor +1
    One big issue is that MS has a requirement that Arm devices running Windows8 must run UEFI firmware and have secure boot enabled, I'll refrain from lighting that particular flame-fest here, but it should…
  • hawkeyethehacker
    hawkeyethehacker over 12 years ago in reply to e14 Contributor +1
    As someone who works on embedded platforms I have two things to say: Please, spell correctly so other people can understand you We know computers work on binary, however the problem is how said computer…
Parents
  • SGarciaV
    0 SGarciaV over 13 years ago

    I agree with Coder27. Since Raspberry Pi runs Linuz the question could changed to "Can Windows xp/8 run on Linux?". Surprisingly, the answer to this yes, but with certain reservations. The hardware that is running the host operatng system, in this case Linux, must have the resources that the client operating system, in this case Windows xp/8, requires.

     

    The Raspberry Pi, in my opinion, is sorely lacking the resources necessary to run Windows XP/8. The 512 MB RAM can run WIndows XP, but the R-Pi lacks the processor horsepower and secondary storage. This device was never meant to host other operating systems, especially those as complex as Windows. Now, if you want to run MS-DOS, that is another matter :-). Regards, Salvador

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • SGarciaV
    0 SGarciaV over 13 years ago

    I agree with Coder27. Since Raspberry Pi runs Linuz the question could changed to "Can Windows xp/8 run on Linux?". Surprisingly, the answer to this yes, but with certain reservations. The hardware that is running the host operatng system, in this case Linux, must have the resources that the client operating system, in this case Windows xp/8, requires.

     

    The Raspberry Pi, in my opinion, is sorely lacking the resources necessary to run Windows XP/8. The 512 MB RAM can run WIndows XP, but the R-Pi lacks the processor horsepower and secondary storage. This device was never meant to host other operating systems, especially those as complex as Windows. Now, if you want to run MS-DOS, that is another matter :-). Regards, Salvador

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to SGarciaV

    Thanks guys. But I have seen such things as mini xp running on a Pi at school but the person will not tell me how they have done it :(. And I also wondered even though (Salvador) you say it lacks 'horsepower' I was interested in the specific topic o windows 8 purely down to that W8 itself claims that it supports ARM processors; as such in portable devices. Is it just that the Pi itself hasn't got the right type ARM processor to be capable of running windows 8? (Forgetting the variables of other hardware such as ram ect...)

     

    Thanks again, Lloyd 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    You can run VNC on linux and make it seem like you're using Windows on a Pi. For example: https://www.youtube.com/watch?v=WYQyUqFck6I

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SGarciaV
    0 SGarciaV over 13 years ago in reply to e14 Contributor

    Yes, you've hit upon an interesting point. When XP is installed (and no doubt applies to newer versions of Windows) it installs many processes that are executed when Windows is nornally running. Some of those process are needed, such as the Windows Explorer, but others are not. What your "friend" did was remove all the unnecesary processes.

     

    By doing this the hardware requirements drop to a point where you can run a minimal install of Windows on scant resources. How useful such an install is is another matter.

     

    Also, there stands the possibility that your friend got this install by following instructions available on the Web.

     

    Here is a link that could get you started: http://www.ehow.com/how_7295926_install-mini-windows-xp.html

     

    Also, look for mini windows xp or minimal windows install for more information. I am sure that you'll come up with other helpful search phrases. There was also a program that would allow you to customize Windows by permitting you to add and remove Windows components and create an install disc. It is called NLITE: http://www.nliteos.com/

     

    I would read about this program before using it, just to be sure that it is something that can help you.

     

    As Coder27 said, some versions of Windows do support ARM, but only specific models and the ARMv6 is not one of them:

     

    http://www.pimpmypi.com/wiki/wikiPage.php?wikiPageID=19&categoryID=1

     

    (You might find some interesting stuff in the above Website.)

     

    Salvador

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SGarciaV
    0 SGarciaV over 13 years ago in reply to e14 Contributor

    That is just plain sneaky! :-) Salvador

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • SGarciaV
    0 SGarciaV over 13 years ago in reply to e14 Contributor

    And 2 more links before I make a hasty retreat:

     

    Run Win XP on R-Pi

    http://www.raspberrypi.org/phpBB3/viewtopic.php?f=56&t=41444

     

    Run Win 7 on R-Pi using VMWare

    http://www.youtube.com/watch?v=ok5sKzlH8es

     

    And another (yes that makes three, I always had problems counting) link to an article that caught my attention, but did not really understand what it is about. It might be something useful, then again maybe not:

    http://www.raspbmc.com/wiki/user/windows-installation/

     

    From quickly glancing over the About page it looks like it is a Linux distrib. Whatever :- Salvador

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    One big issue is that MS has a requirement that Arm devices running Windows8 must run UEFI firmware and have secure boot enabled, I'll refrain from lighting that particular flame-fest here, but it should be easy to find with a little googling.

     

    Suffice to say that the Pi doesn't have UEFI and you'd need either broadcom or the RPF to implement it.

     

    So regardless of any theoretical possibility that the cpu on the Pi could be capable of running Win8, if you're unable to boot the OS to begin with it's all rather academic.

     

    There are many other issues to consider, things like it appears that the only way to get Win8 for Arm will be pre-installed on some device. So you'd have to consider if a version of Win8 customised for a different piece of hardware would even run on the Pi, have the correct drivers etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to SGarciaV

    Thanks again Salvador :D you have been a massive help and I will take a look at those links.

    Kind regards, Lloyd

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Russell Martelli wrote:

     

    You can run VNC on linux and make it seem like you're using Windows on a Pi.

    You don't need VNC, windows comes with it's own remote desktop functionality and most linux distros come with the 'rdesktop' application that's used to remotely connect to a windows desktop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Oh cool, I didn't know that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to SGarciaV

    you are all rong as a programer in it i understand that operating systems work on 01 (bianary) if you downlode mac you run 01 to run funchons linik 01 and windows 01 if you were to use windows you have to make it so its on the harddrive by the logic you are explaning you can have linix on a mac and mac cant read webpages that are in windows html and linix cant script for a windows so you ship is bull crafp kid find some one else to talk to it may tack yeasrs but find a emulater that runs on the rasberian and makes a program that acts like windows 7 it adds a exer os for you and you can run it in your hot line to save cpu and cpu is rong it will only run wut its got to get more cup just get a bigger hard drive for example 8 gb isent enuff get a 64 gb then a tarabight external hardrive to confinscat for the lack of ran and your good