• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Ultimate alarm clock
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 28 subscribers
  • Views 183 views
  • Users 0 members are here
  • hardware
  • build_challenge
  • idea
  • viewer_challenge
  • ben_heck
  • show_idea
Related

Ultimate alarm clock

joecr
joecr over 13 years ago

I'm thinking about making an alarm clock as none of models I see in stores have all the features I want. I was thinking some of the features could be upgrades that you connect while the clock is off.

Here are some features I've thought of so far in no particular order.

  • Auto-snooze (If you don't hit the snooze button in x seconds it will assume you want it to snooze.)
  • Color selection for display. (Could also include fine level brightness controls. RGB LEDs or LCD screen. I have a friend that wants his alarm clock to have a purple display.)
  • Multiple alarm sounds (Also allow custom alarm sounds.)
  • Battery powered (Some features might need to be disabled on battery power.)
  • Auto time set (Either through the Internet or at least in the lower 48 states use the Colorado nuclear time clock.)
  • Web interface to program alarms, & upload alarm sounds & make changes to device settings. (Password protected)
  • Version for hotels when guest requests a wake-up call to have a recording play to wake them up. (The alarm clock could call the worker to remind them that the room X wanted a wake-up call.)
  • For hotels in the lower 48 a device that will pickup the time from the Denver Colorado Nuclear time clock to broadcast over hotels network. (Some buildings construction could block the signal from the individual alarm clocks.)
  • Line in for speakers to play from any audio device.
  • Multiple USB ports for charging devices with a 5 volt & 2 Amps per port & configured to work with devices like the iPhone.
  • HD radio.
  • Internet radio apps, Pandora, Last.fm, etc…
  • Day of the week & date on display. (Could be just a button to display it.)
  • Can tell the temperature. (With a local & a remote sensor.)
  • Ability to tell time verbally.
  • Option to have display dot matrix or the more traditional digital display format.
  • Ability to have a custom enclosure made.
  • When powered on upgrade door(s) are auto closed until power is lost.

Some questions about options to do a feature.

  • For time zone should it be set by a switch or stored on SD card & also if DST is used. Which way should it be done?
  • Would you want a solar panel on a battery only version?
  • Should the web interface WordPress with a plugin be used for the interface or something else?

Are there any ideas you want to add?

I'm also thinking about making the hardware open source & using as much open source hardware as possible, unless a closed source chip is cheaper I might use that instead.

 

I did post this over at my blog the post is Ultimate alarm clock.