• Products and Partners
    Products and Partners
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How possible is it to make a wireless 360 controller into a wired one for use on PC?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 34 subscribers
  • Views 8639 views
  • Users 0 members are here
  • 360
  • controller
  • wired
  • wireless
Related

How possible is it to make a wireless 360 controller into a wired one for use on PC?

e14 Contributor
e14 Contributor over 13 years ago

Just like the title says, would it be possible to make a wireless 360 controller into a wired controller for use on a pc? I'm tired of getting the charge packs that just stop charging after a while or after they get glitched up.

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • elevatorguy
    elevatorguy over 13 years ago +1
    The hard way: If you are comfortable with soldering and like to take the controller apart, then it is possible, for example, to open up the controller, solder wires from buttons, trigger and joystick potentiometers…
Parents
  • elevatorguy
    0 elevatorguy over 13 years ago

    The hard way:

    If you are comfortable with soldering and like to take the controller apart, then it is possible, for example, to open up the controller, solder wires from buttons, trigger and joystick potentiometers, coming out to where the battery pack used to be, and put a teensy there acting as a USB HID gamepad to the computer, wiring the power and ground from the teensy to the gamepad, to power it. (I would double check the voltages, but it's probably 3.3V on both)

     

    Additionaly, it could be possible to still use it with the xbox 360, it would work wirelessly, but using the USB for power. If we are not interfaceing with a chip in the xbox gamepad, but reading the buttons and pots directly (easier programming, but 21 wires), then technically it could be used with both at the same time. We'd have to use pretty thin wires, to fit it all in there. I havn't modded a 360 controller, but when I did a N64 controller like this, it was interesting getting it back together. But in the end, I had a N64 controller that I made myself that showed up as a USB gamepad on the computer.

     

    It's alot of work, but if interested, then it can be a fun and rewarding project image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to elevatorguy

    I'm good at soldering, so that wouldn't be a problem. I was thinking that there might be existing circuitry that can be used, because the pc recognizes a 360 controller plugged in when using the play and charge cable. Sadly, it does not operate like a wired controller when you have it plugged into the pc using the charge cable.

     

    edit:

    maybe these pcbs can help out, it's interesting that the sync button is labeled as "wire/wireless plug switch"

     

    wired pcb

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram6.jpg

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram1.jpg

     

     

    wireless pcb

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram5.jpg

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram7.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to elevatorguy

    I'm good at soldering, so that wouldn't be a problem. I was thinking that there might be existing circuitry that can be used, because the pc recognizes a 360 controller plugged in when using the play and charge cable. Sadly, it does not operate like a wired controller when you have it plugged into the pc using the charge cable.

     

    edit:

    maybe these pcbs can help out, it's interesting that the sync button is labeled as "wire/wireless plug switch"

     

    wired pcb

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram6.jpg

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram1.jpg

     

     

    wireless pcb

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram5.jpg

    http://www.slagcoin.com/joystick/pcb_diagrams/360_diagram7.jpg

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • joecr
    0 joecr over 13 years ago in reply to e14 Contributor

    Way to much work & it wouldn't really be cost efective. Just go to the store & buy a wired controller. It's easier & faster than setting everything to use a teensy.