element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Strange Behavior with 20*4 LCD (BASIC-Computer with Arduino)
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 30 subscribers
  • Views 1234 views
  • Users 0 members are here
  • lcd
  • computer
  • episode
  • retro
  • ben_heck
  • basic
  • ben
  • arduino
Related

Strange Behavior with 20*4 LCD (BASIC-Computer with Arduino)

e14 Contributor
e14 Contributor over 13 years ago

I already posted about this issue in this thread, but I think, my issue is different.

I have changed ca. 10-15 lines in the original source code provided by Ben Heck. The 20*4 LCD now outputs Data without line-problems, but the 4 characters in the topright corner are displayed at the beginning of the third line!?

It looks like this:

                    
TinyBasic
1146 Free.
>10 print "1234567"_

TinyBasic           
1146 Free
>10 print "1234567"
>_

1146 Free.
>10 print "1234567"
>
>_

>10 print "12345
>
>7"
>_

in the fourth frame, after pressing LF, until the entered command goes up to the first line, only the left 16 chars are shown (the rest are blanked out), and the other 4 are in the third line, although the 17th is overwritten by the cursor > (in fact, up to all 4 could be overwritten if something would be written in this line)

Does anyone knows how to fix this? I am desperately trying to figure this out.

I marked the changes I made in the source code in the link in the first line in this post. I don't know if I am allowed to post the script here.

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The chip that drives the LCD has a characters memory of 4 lines and 40 characters for each line.

    That is happening because this chip is used in a variety of LCD screens.

    Yours is only 20 characters long for each line so you can write the first 20 letters and then you have to change line by adding + 21 because the first memory address is the zero "0" not the 1.

    at least as far as I can remember the 40 th by number memory address must probably be the first character of the

    SECOND LINE.

    So the first character of the third line is the 80th by DECIMAL NUMBER memory address.

    And the forth's line first memory DECIMAL number is 120.

    So the last memory address is 159 decimal.

    The program should have 4 loops of the For (  ) {  } each one loading an array of characters with the size of 19

    because arrays begin too from 0 not 1 because in a binary system the very first state is the zero in all of it's bits.

     

    allways search for the manual of the chip you are trying to use in a circuit board.

     

    I think I helped you a lot but try to look at the chips manual for any different numerical assignment of the addresses. But I believe I remember right the way this 30+ years old chip in the LCD DISPLAY functions.

     

    Message was edited by: Gerasimos Kokkinos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The chip that drives the LCD has a characters memory of 4 lines and 40 characters for each line.

    That is happening because this chip is used in a variety of LCD screens.

    Yours is only 20 characters long for each line so you can write the first 20 letters and then you have to change line by adding + 21 because the first memory address is the zero "0" not the 1.

    at least as far as I can remember the 40 th by number memory address must probably be the first character of the

    SECOND LINE.

    So the first character of the third line is the 80th by DECIMAL NUMBER memory address.

    And the forth's line first memory DECIMAL number is 120.

    So the last memory address is 159 decimal.

    The program should have 4 loops of the For (  ) {  } each one loading an array of characters with the size of 19

    because arrays begin too from 0 not 1 because in a binary system the very first state is the zero in all of it's bits.

     

    allways search for the manual of the chip you are trying to use in a circuit board.

     

    I think I helped you a lot but try to look at the chips manual for any different numerical assignment of the addresses. But I believe I remember right the way this 30+ years old chip in the LCD DISPLAY functions.

     

    Message was edited by: Gerasimos Kokkinos