element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Strange Behavior with 20*4 LCD (BASIC-Computer with Arduino)
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 30 subscribers
  • Views 1234 views
  • Users 0 members are here
  • lcd
  • computer
  • episode
  • retro
  • ben_heck
  • basic
  • ben
  • arduino
Related

Strange Behavior with 20*4 LCD (BASIC-Computer with Arduino)

e14 Contributor
e14 Contributor over 13 years ago

I already posted about this issue in this thread, but I think, my issue is different.

I have changed ca. 10-15 lines in the original source code provided by Ben Heck. The 20*4 LCD now outputs Data without line-problems, but the 4 characters in the topright corner are displayed at the beginning of the third line!?

It looks like this:

                    
TinyBasic
1146 Free.
>10 print "1234567"_

TinyBasic           
1146 Free
>10 print "1234567"
>_

1146 Free.
>10 print "1234567"
>
>_

>10 print "12345
>
>7"
>_

in the fourth frame, after pressing LF, until the entered command goes up to the first line, only the left 16 chars are shown (the rest are blanked out), and the other 4 are in the third line, although the 17th is overwritten by the cursor > (in fact, up to all 4 could be overwritten if something would be written in this line)

Does anyone knows how to fix this? I am desperately trying to figure this out.

I marked the changes I made in the source code in the link in the first line in this post. I don't know if I am allowed to post the script here.

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • benheck
    0 benheck over 13 years ago

    Some RAM is set aside as "screen memory" in that code. It is then mapped to the display.

     

    Check that enough has been allocated, since youre display is larger than the one I used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to benheck

    Xg ++ should be put inside the loop and not in the declaration of the For (  ){ }

    That is because your variable enters the loop already added by one "1" so the loop begins with your variable higher by one more than you expected to be.

    So instead of beginning with zero it begins with one so you have 19 repeats not 20.

    All of my posts refer to the C++ language ,for the basic as language adjust accordingly.


     

    Message was edited by: Gerasimos Kokkinos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to benheck

    Xg ++ should be put inside the loop and not in the declaration of the For (  ){ }

    That is because your variable enters the loop already added by one "1" so the loop begins with your variable higher by one more than you expected to be.

    So instead of beginning with zero it begins with one so you have 19 repeats not 20.

    All of my posts refer to the C++ language ,for the basic as language adjust accordingly.


     

    Message was edited by: Gerasimos Kokkinos