element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum I want to build a car parked detector for my garage
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 17 replies
  • Answers 2 answers
  • Subscribers 34 subscribers
  • Views 1954 views
  • Users 0 members are here
Related

I want to build a car parked detector for my garage

gez
gez over 13 years ago

Hi,

 

Does anyone know how those car detectors work in shopping center carparks? You know the ones that show a green or red light depending on whether a car is parked in the space. I want to make one that will tell my phone if a car is parked in the garage or not. I was thinking of using an arduino connected to a"Ultrasonic Module HC-SR04 Distance Measuring Transducer Sensor for Arduino measurer" to measure the distance from the ceiling to the floor/top of the car, but someone said they thought they worked by using a magnetic field.

 

Gez

  • Sign in to reply
  • Cancel
Parents
  • benheck
    0 benheck over 13 years ago

    A 38KHz detector could work, but sometimes they're TOO sensitive. Think of your TV remote, which works even if you bounce it off your eyeball or teeth.

     

    Ultrasonic sounds like a good bet! You can get distance with that too, not just blocked/unblocked.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gez
    0 gez over 13 years ago in reply to benheck

    Yeah, I have decided to try using two ultrasonic measurers, a RGB LED and an arduino; I will use one sensor to detect if a car is parked in the space, the other to detect if a car parks in the driveway. I'm thinking that I can use some logic like:

     

    The driveway sensor detects that a car has entered the driveway because the distance to the driveway has shortened by x amount from y, and remains shortened for longer than z seconds. This should prevent false positives caused by someone walking past the sensor.

     

    Read the sensor in the garage to determine if a car is parked there.

     

    Flash an RGB LED on the garage door for a predetermined number of seconds, green if no car is parked there, red if there is.

     

    Reset the sequence when the distance to the driveway returns to its default y value.

     

    Sounds simple image If my sensors arrive soon I might get it done this weekend!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • gez
    0 gez over 13 years ago in reply to benheck

    Yeah, I have decided to try using two ultrasonic measurers, a RGB LED and an arduino; I will use one sensor to detect if a car is parked in the space, the other to detect if a car parks in the driveway. I'm thinking that I can use some logic like:

     

    The driveway sensor detects that a car has entered the driveway because the distance to the driveway has shortened by x amount from y, and remains shortened for longer than z seconds. This should prevent false positives caused by someone walking past the sensor.

     

    Read the sensor in the garage to determine if a car is parked there.

     

    Flash an RGB LED on the garage door for a predetermined number of seconds, green if no car is parked there, red if there is.

     

    Reset the sequence when the distance to the driveway returns to its default y value.

     

    Sounds simple image If my sensors arrive soon I might get it done this weekend!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 13 years ago in reply to gez

    Gerry

     

    Mapping out how it should work is the first part of the puzzle, and is often missed by newcomers to programming.

    I suggest using the millis() for timing rather than delay() as it allows you to continue doing other things.

     

    It should be a good project, and you should start a blog, to allow others to follow.

    It doesn't need to be a single, it can have additions made as you solve issues, add features.

    (unfortunately its last in at the top, so following it works from the bottom)

     

    eg http://www.element14.com/community/people/mcb1/blog/2013/08

     

    Mark