Products
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
element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Webcam mod for astrophotography
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 31 subscribers
  • Views 1770 views
  • Users 0 members are here
  • astrophotography
  • astronomy
  • heck
  • ben
Related

Webcam mod for astrophotography

e14 Contributor
e14 Contributor over 12 years ago

Dear Ben

 

I am an amateur astronomer and have an interest in Astrophotography.

Can you help me to create a mod to take long exposure pictures using a webcam like the Philips SPC900NC.

Maybe a mod using a raspberry pi or an other equivalent controler. (if possible)

 

Thank you in advance

 

WIth regards yiangos.

  • Sign in to reply
  • Cancel
Parents
  • ckraft
    0 ckraft over 12 years ago

    I am building something similar for my telescope. I took a Microsoft HD webcam as the starting point, because the existing shape. I am going to 3D print an adapter so it fits into the telescope snugly and then I plan to come up with some mechanism to get the data back via WiFi. I plan to also use this as a platform for remote control of the telescope so that I don't have to sit outside in the cold Wisconsin Winter which is usually the best viewing time around here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ckraft
    0 ckraft over 12 years ago

    I am building something similar for my telescope. I took a Microsoft HD webcam as the starting point, because the existing shape. I am going to 3D print an adapter so it fits into the telescope snugly and then I plan to come up with some mechanism to get the data back via WiFi. I plan to also use this as a platform for remote control of the telescope so that I don't have to sit outside in the cold Wisconsin Winter which is usually the best viewing time around here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to ckraft

    WOW!  i really hope everything goes the way you want. although i would like to remind you to check the lowest light the specific camera will work in.

    you may have a problem using it in low light. your best shot would be to get a camera that has a CCD chip.

    do you know if it is possible to create your own camera using materials on element14?

    for example create a custom system with the CCD of your choice

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 12 years ago in reply to ckraft

    Hi Chris,

     

    I have seen a couple of mods using the Microsoft HD camera with really good results.

    Some have removed the lens and then gone with critical focus, while others have used adapter tubes and done eyepiece projection.

    It mostly depends upon the types of objects you want to take in and at what resolution.

    The eyepiece projection method has the most flexibility for small objects, but the prime focus is useful for large objects like the moon or the sun.

     

    I have the microsoft camera and have used it for lightning photos.  It takes a bit of work to get the setting correct, but the quality has been very good.

     

    I have also seen some posts on the web about setting up an automated telescope.

    I sympathise about the cold weather.  I am in west central Ohio and it gets a bit nippy in the dark winter months.

     

    Good luck,

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 12 years ago in reply to e14 Contributor

    Hi Yiangos,

     

    I recommend that you first try with an inexpensive web camera and try the eyepiece projection method.  All you need is an adjustable tube assembly, cardboard tubes work just fine, and then work out the focal length that you want to try.

    There are several software programs that you can use with the web cam to play with exposure.

    The aperature size of your scope will also impact what you can expect to see.  That is why I suggest trying out a simple implementation.  You might have to go to either a larger scope or a less pixel sized camera to get the best results.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ckraft
    0 ckraft over 12 years ago in reply to DAB

    I removed the lens and IR filter from the camera, at least I think I removed the IR filter, and am 3D printing an adapter so it can go into where the eye-piece would be.

     

    I would love to go CCD but that's a bit beyond my budget right now. I just wanted to try something a step up from what I have now, which is basically nothing.

     

    I thought about the possibility of DIYing a CCD unit, I did some initial research on CCD chips but that's well outside my prior experience so I don't know. I imagine most of the parts are available from Element-14 but I wouldn't know where to start myself. It would be an impressive project though.

     

    I am mostly just following guides I found online. My stuff is no-where near the level of some of what some people have built. I am just getting started. Most of my current effort is in reverse engineering the GPS control on the Celestron telescope control.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 12 years ago in reply to ckraft

    Hi Chris,

     

    I know that Celestron used to provide some of the protocols for people to integrate the positioning system with an external PC control.

    You might want to contact them to see if they have an SDK you can use.

     

    Removing the IR filter will screw up the autofocus controlled by the firmware, but you should be able to manually adjust both the focus and the exposure times.

    I just used the Microsoft manual control and it worked pretty good once you figure out what they have done.

    It looks like they used software people to write a camera control software without first having photographers around to make the controls sound like normal camera lingo.

     

    Are you planning to use bandpass filters for your data collection.  Without the IR filter, the Red pixels will be a bit too bright and shift the color balance a tad.  If you have photoshop or Gimp, you can easily correct for the change.

     

    Sounds like a fun project.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to DAB

    HI

    I already have 2 SPC-900 webcams with a CCD chip which i use for planetary lunar or sun observation in various configuration including A-focal as you have described.

    now i am bored with planets and want to capture Deep Space Objects, something that can be done taking long exposure pictures.

    the problem with the CCD i have is the low resolution. the next best step would be to buy a DSLR camera which has certain limitations, for ex. the IR filter in the camera which i would have to remove.

    its like saying to yourself pay 1000 dollars to buy one and then take apart. (i'm kinda not up for that) and then not being able to use it as an everyday camera.

    So i'm looking for a project to engage in my spare time. the use of the Raspberry Pi with its camera board ans suggested by Scott does sound interesting and is worth a look.

    thank for the advice though..