element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Coordinated Stepper Motor motion factoring Aceel/Decel for arduino
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 32 subscribers
  • Views 1281 views
  • Users 0 members are here
Related

Coordinated Stepper Motor motion factoring Aceel/Decel for arduino

timryder
timryder over 12 years ago

Ok so I'm creating a machine for myself and its going to be like an X,Y CNC with a possible A axis rotary.

What I want to do with it is write the code from scratch to so it's lean and fast. I might not be able to achieve this but it's going to serve as both a learning tool and a functional product for me to use.

 

I've been doing some experimenting controlling stepper motors with an Arduino Mega 2560 and I've had some success with an Arduino Library called "AccelStepper".  This is a pretty handy library which allows me to control multiple steppers and many types of drivers or direct. What it lacks however and is the most important is a canned function  which would allow me to coordinate motion of multiple axis factoring in their Accel and Decel profiles. If you haven't dealt with this at all it's a huge pain in the but because stepper motors unlike a dc brush less motor are digital, that is they can't take an analog motion profile.  Given their digital nature the standard trapezoid model of accel/decel won't work as each step of the stepper motor will/may be greater than the distance over time desired to match the rise/run profile of the accel/decel.  So what I usually end up with is the axis with the shorter move finishes it's motion faster than the longer motion axis.

 

Does anyone out there have any experience solving this dilemma?  I've tried some simple equations all of which would work for an analog device but I'm not gaining any ground on this battle at the moment.

 

If anyone needs more information I can do a video or some sort of diagram.


Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    If you are using arduino, then is shouldn´t be a problem.Try to write some examples first, to drive steppers, then try to write all logic that it needs to preform tasks.

    At the end, combine all those into one .ino file. Write a function for all axis and then try to combine all together. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    If you are using arduino, then is shouldn´t be a problem.Try to write some examples first, to drive steppers, then try to write all logic that it needs to preform tasks.

    At the end, combine all those into one .ino file. Write a function for all axis and then try to combine all together. image