element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Coordinated Stepper Motor motion factoring Aceel/Decel for arduino
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 32 subscribers
  • Views 1280 views
  • Users 0 members are here
Related

Coordinated Stepper Motor motion factoring Aceel/Decel for arduino

timryder
timryder over 12 years ago

Ok so I'm creating a machine for myself and its going to be like an X,Y CNC with a possible A axis rotary.

What I want to do with it is write the code from scratch to so it's lean and fast. I might not be able to achieve this but it's going to serve as both a learning tool and a functional product for me to use.

 

I've been doing some experimenting controlling stepper motors with an Arduino Mega 2560 and I've had some success with an Arduino Library called "AccelStepper".  This is a pretty handy library which allows me to control multiple steppers and many types of drivers or direct. What it lacks however and is the most important is a canned function  which would allow me to coordinate motion of multiple axis factoring in their Accel and Decel profiles. If you haven't dealt with this at all it's a huge pain in the but because stepper motors unlike a dc brush less motor are digital, that is they can't take an analog motion profile.  Given their digital nature the standard trapezoid model of accel/decel won't work as each step of the stepper motor will/may be greater than the distance over time desired to match the rise/run profile of the accel/decel.  So what I usually end up with is the axis with the shorter move finishes it's motion faster than the longer motion axis.

 

Does anyone out there have any experience solving this dilemma?  I've tried some simple equations all of which would work for an analog device but I'm not gaining any ground on this battle at the moment.

 

If anyone needs more information I can do a video or some sort of diagram.


Thanks!

  • Sign in to reply
  • Cancel
Parents
  • ckraft
    0 ckraft over 12 years ago

    Wish I could help but If I need lean/decent stepper control on an Arduino I usually use grbl (Bengler: GRBL) which is very nice and very lean, even runs on a standard Arduino.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • timryder
    0 timryder over 12 years ago in reply to ckraft

    Chris!

     

    You nailed it with GRBL, I took sections from it's AVR_C and made my own using it as inspiration. Very cool program.

    Now when you write a program with AVR_C and compile it, does it run faster than using one written through the Arduino IDE?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • timryder
    0 timryder over 12 years ago in reply to ckraft

    Chris!

     

    You nailed it with GRBL, I took sections from it's AVR_C and made my own using it as inspiration. Very cool program.

    Now when you write a program with AVR_C and compile it, does it run faster than using one written through the Arduino IDE?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • ckraft
    0 ckraft over 12 years ago in reply to timryder

    If you write the C-code yourself it has the potential to be faster than the Arduino code but it is not a guarantee. Ultimately the Arduino code at some point ends up compiled code so there is not an obvious difference in performance. Plus odds are that you and the Arduino code are compiling in/linking the same libraries from Atmel/AVR so there won't be much difference there.

     

    That said when you write the code yourself you have the ability for tighter control over what code is there and how it is structured. So if the Arduino tool is doing something stupid for the sake of consistency between platforms you can make your code more efficient.

     

    It is a great exercise to learn more about the platform. That's why I encourage people using the Arduino tool to dig under the surface and take a look at the code it generates to better understand what is going on.