element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum beagle bone black current meter
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 31 subscribers
  • Views 1343 views
  • Users 0 members are here
  • current
  • meter
  • BeagleBone
Related

beagle bone black current meter

e14 Contributor
e14 Contributor over 12 years ago

I'm going to try and make a current monitor on the beagle bone, but a single adc dosn't have enough resolution for me so I want to use 4 of the beagles adc pins with a quad opamp to amplify the voltage to separate bands and a couple of transistors to keep the max value to the beagles 1.8V adc reference voltage. the range of current i want to measure would be 0-100mA at 3.6V. I have the programming skills but not the faith in my hardware knowledge so if anyone wants to help me with tips or component lists, It would be appreciated.

  • Sign in to reply
  • Cancel
Parents
  • vsluiter
    0 vsluiter over 12 years ago

    Why not use the very simple devices by Zetex? They're quite small, already have a built-in gain, or a current output (so you can set the gain by adding an external resistor). Take a look at ZXCT1041 (bidirectional, gives absolute value of current) or ZXCT1109 (1-directional, is supplied by sense voltage. Ideal for monitoring a power line).

    Touchstone also provides these sensors, and ships free samples (Current Sense Amplifiers | Touchstone Semiconductor)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vsluiter
    0 vsluiter over 12 years ago

    Why not use the very simple devices by Zetex? They're quite small, already have a built-in gain, or a current output (so you can set the gain by adding an external resistor). Take a look at ZXCT1041 (bidirectional, gives absolute value of current) or ZXCT1109 (1-directional, is supplied by sense voltage. Ideal for monitoring a power line).

    Touchstone also provides these sensors, and ships free samples (Current Sense Amplifiers | Touchstone Semiconductor)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to vsluiter

    There might be some problems with the '1041 because its output impedance is 15k but the suggestion in the BBB docs is that the source impedance be less than 1k. It's in surface mount as well but the OP hasn't said if that's a problem.

    The high side sensing ability might be useful.

     

    MK