element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum beagle bone black current meter
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 1 answer
  • Subscribers 31 subscribers
  • Views 1342 views
  • Users 0 members are here
  • current
  • meter
  • BeagleBone
Related

beagle bone black current meter

e14 Contributor
e14 Contributor over 12 years ago

I'm going to try and make a current monitor on the beagle bone, but a single adc dosn't have enough resolution for me so I want to use 4 of the beagles adc pins with a quad opamp to amplify the voltage to separate bands and a couple of transistors to keep the max value to the beagles 1.8V adc reference voltage. the range of current i want to measure would be 0-100mA at 3.6V. I have the programming skills but not the faith in my hardware knowledge so if anyone wants to help me with tips or component lists, It would be appreciated.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    thanks all for your input, package isn't that much of a problem as-long as is big enough to solder by hand though Id prefer through hole components,

    to Michael Kellett, I read that it was an 8bit but further reading has shown me that too, so 1 ADC may well be enough but your comment on a second amp wouldn't give me any advantage as it will still have the same 0 and thus id only get increased resolution on the low end but I did find a possibility if I add a reference voltage to the signal and put them in a negative of an opamp then the wave is shifted down allowing me to start the second from 1/2 the hight of the wave and thanks for the heads up on the ZXCT1041 I'm not sure what the problem is with impedance if you could give me a point in the right direction regarding the docs.

     

    Thanks again all

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    thanks all for your input, package isn't that much of a problem as-long as is big enough to solder by hand though Id prefer through hole components,

    to Michael Kellett, I read that it was an 8bit but further reading has shown me that too, so 1 ADC may well be enough but your comment on a second amp wouldn't give me any advantage as it will still have the same 0 and thus id only get increased resolution on the low end but I did find a possibility if I add a reference voltage to the signal and put them in a negative of an opamp then the wave is shifted down allowing me to start the second from 1/2 the hight of the wave and thanks for the heads up on the ZXCT1041 I'm not sure what the problem is with impedance if you could give me a point in the right direction regarding the docs.

     

    Thanks again all