element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum arduino hack
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 30 subscribers
  • Views 535 views
  • Users 0 members are here
Related

arduino hack

royston02
royston02 over 12 years ago

I have brought the arduino pro mini. It's IO pins gives 5V. I wanted 3.7V. There's an onboard voltage regulator mic5025 and has 5 pins. I wanted to know if I can cut the traces and add a 3.7V regulator and if  so what precautions must be taken. Also I can't use the 3.3V  arduino pro mini cause I required 3.7 V only and no lesser.

  • Sign in to reply
  • Cancel
Parents
  • Workshopshed
    0 Workshopshed over 12 years ago

    The key difference between the 3.3v and 5v versions is the timing crystal. The higher voltage allows it to run at a higher clock speed, this also means the bootloader software in the chip is coded to work with that speed so functions like millis are correctly calibrated. I suspect that trying to run a 3.7v with the higher speed will lead to instability.

     

    Starting from where you are I'd use a voltage booster module or chip to get your supply upto 5v to run the pro mini and then use a level shifter circuit (perhaps a simple resistor voltage divider might work) to ensure that the outputs toggle between 0 and 3.7v. If you are communicating at a higher speed then you might need a more sophisticated circuit.

     

    Alternatively use a 3.3v device and use transistors to boost the output voltage of the I/O

     

    Also check the data sheets of the device you are connecting to. For example a some of the Ethernet chips have a 3.3v supply but can work correctly even if the data lines are at 5v. So you might find you can use your circuits without change.

     

    Level Shifting Digital Signals - Application Note - Maxim

    Incredible DIY: Simple 3.3V–5V level shifter

    Code and Life – Level Shifting 101

    Voltage booster Product LinkProduct Link

     

    Here's a page that looks at power saving. It does suggest running at lower voltages is a possibility. For 16Mz (the clock speed of the 5v) version it recommends 3.78v so you might just find you can get away with it.

     

    Electronics : Microprocessors : Power saving techniques for microprocessors

     

    You just connect the supply voltage to VSS (rather than RAW), no need to cut any tracks.

     

    Note for programming etc you probably want to use 5v.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Workshopshed
    0 Workshopshed over 12 years ago

    The key difference between the 3.3v and 5v versions is the timing crystal. The higher voltage allows it to run at a higher clock speed, this also means the bootloader software in the chip is coded to work with that speed so functions like millis are correctly calibrated. I suspect that trying to run a 3.7v with the higher speed will lead to instability.

     

    Starting from where you are I'd use a voltage booster module or chip to get your supply upto 5v to run the pro mini and then use a level shifter circuit (perhaps a simple resistor voltage divider might work) to ensure that the outputs toggle between 0 and 3.7v. If you are communicating at a higher speed then you might need a more sophisticated circuit.

     

    Alternatively use a 3.3v device and use transistors to boost the output voltage of the I/O

     

    Also check the data sheets of the device you are connecting to. For example a some of the Ethernet chips have a 3.3v supply but can work correctly even if the data lines are at 5v. So you might find you can use your circuits without change.

     

    Level Shifting Digital Signals - Application Note - Maxim

    Incredible DIY: Simple 3.3V–5V level shifter

    Code and Life – Level Shifting 101

    Voltage booster Product LinkProduct Link

     

    Here's a page that looks at power saving. It does suggest running at lower voltages is a possibility. For 16Mz (the clock speed of the 5v) version it recommends 3.78v so you might just find you can get away with it.

     

    Electronics : Microprocessors : Power saving techniques for microprocessors

     

    You just connect the supply voltage to VSS (rather than RAW), no need to cut any tracks.

     

    Note for programming etc you probably want to use 5v.