element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum [pinball] how about a Pi-based pinball driver board?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 28 subscribers
  • Views 258 views
  • Users 0 members are here
Related

[pinball] how about a Pi-based pinball driver board?

e14 Contributor
e14 Contributor over 12 years ago

Hi everyone

My pinball fascination began with TBHS episode about it, since then, i was thinking about a way to make driver boards simplier (2+ microcontrollers and 3+ sd cards - it`s not a mess, but still too much if you ask me)

Solution i came up with: unification using Raspberry Pi - just make a driver board with a slot for Pi, then you have (with model B):
- 700mhz/512mb that is more than enough to drive everything in pinball (and it`s still not a PC, but embedded device, so it`s not an overkill)

- low level connections: 8 × GPIO, UART, I²C bus, SPI bus with two chip selects, I²S audio +3.3 V, +5 V

- 2xUSB, so you can extend driver connection capabilities (this idea came from P-ROC/P3-ROC)

- Ethernet for remote control, program management and other "bonus" features

- video output - maybe THIS is overkill, but i think this would be useful in some situations (like a multiplayer scorekeeping w/o multiple LED panels or color animations)

- 3,5mm jack - for me, that`s the simpliest way to stereo audio

- built-in SD card slot, so you can store all the needed data in one card (which is great, considering that`s cheaper and more failsafe than multi-card solution)

I think that`s a good idea, but i want to know your opinion about it.

 

P,S,: While i was writing text above, i found about Pi Compute Module and that`s even better, because all that`s needed to be soldered on main board is a single SO-DIMM slot