element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Stepper Motor Troubleshooting
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 44 replies
  • Subscribers 33 subscribers
  • Views 7348 views
  • Users 0 members are here
  • help
  • 3d
  • me
  • tags
  • stepper
  • stuff
  • help!
  • printing
  • motor
  • heck
  • ben
Related

Stepper Motor Troubleshooting

fuzion_reaktor
fuzion_reaktor over 12 years ago

Hello, my name is Peter R and for the past several months I have been building a 3D printer. I have the frame and everything done, but I consistently run into the issue where my stepper motors run erratically; when I issue a movement command they change direction at random, move in unpredictable spurts, clank, grind and make weird noises--and that's if I'm lucky enough to get them running at all. They appear to be uni-polar motors, and I have wired their four wires in as many orientations as possible and still get the same issue? Is this a board problem, or the motors themselves?

The motors are 17H249-02S motors, manufactured by Xuquan motor, but there is little documentation on them on the internet as far I have found.

Many thank to whoever can answer this.

  • Sign in to reply
  • Cancel

Top Replies

  • fuzion_reaktor
    fuzion_reaktor over 12 years ago in reply to D_Hersey +2
    Huzzah (yes I say huzzah) I have inadvertently solved my problem. My end-stops were wired improperly so the control board thought that they were closed. Thus my motors could never move in the direction…
  • fuzion_reaktor
    fuzion_reaktor over 12 years ago in reply to kidiccurus +1
    Motors, yes are a plugging in problem. This is just weird. But switching the two works and I have successfully printed a small misshaped cube...Progress...
Parents
  • ootbrobo
    0 ootbrobo over 12 years ago

    What voltage are you powering the motor drivers with?  The board you have contains a chopper drive, which more or less means your driver controls how much current can be delivered to the motors regardless of the motor voltage.  The major benefit is that you can apply higher voltages, which improve the step response of your motors.  What I suspect is that you are running the motors too fast for the voltage you are providing.  Likewise if you are micro-stepping, the motor could be spazzing out, from the torque load.  Stepper torque outputs I believe exponentially decrease with the number of micro-steps.  Last bit, when you transition from stop to start, or direction changes etc.  you need to ramp the motor up to speed.  If you are simply telling the motor to move full speed from a dead stop, you are going to have these kinds of issues.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ootbrobo
    0 ootbrobo over 12 years ago

    What voltage are you powering the motor drivers with?  The board you have contains a chopper drive, which more or less means your driver controls how much current can be delivered to the motors regardless of the motor voltage.  The major benefit is that you can apply higher voltages, which improve the step response of your motors.  What I suspect is that you are running the motors too fast for the voltage you are providing.  Likewise if you are micro-stepping, the motor could be spazzing out, from the torque load.  Stepper torque outputs I believe exponentially decrease with the number of micro-steps.  Last bit, when you transition from stop to start, or direction changes etc.  you need to ramp the motor up to speed.  If you are simply telling the motor to move full speed from a dead stop, you are going to have these kinds of issues.