element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Stepper Motor Troubleshooting
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 44 replies
  • Subscribers 33 subscribers
  • Views 7364 views
  • Users 0 members are here
  • help
  • 3d
  • me
  • tags
  • stepper
  • stuff
  • help!
  • printing
  • motor
  • heck
  • ben
Related

Stepper Motor Troubleshooting

fuzion_reaktor
fuzion_reaktor over 12 years ago

Hello, my name is Peter R and for the past several months I have been building a 3D printer. I have the frame and everything done, but I consistently run into the issue where my stepper motors run erratically; when I issue a movement command they change direction at random, move in unpredictable spurts, clank, grind and make weird noises--and that's if I'm lucky enough to get them running at all. They appear to be uni-polar motors, and I have wired their four wires in as many orientations as possible and still get the same issue? Is this a board problem, or the motors themselves?

The motors are 17H249-02S motors, manufactured by Xuquan motor, but there is little documentation on them on the internet as far I have found.

Many thank to whoever can answer this.

  • Sign in to reply
  • Cancel

Top Replies

  • fuzion_reaktor
    fuzion_reaktor over 12 years ago in reply to D_Hersey +2
    Huzzah (yes I say huzzah) I have inadvertently solved my problem. My end-stops were wired improperly so the control board thought that they were closed. Thus my motors could never move in the direction…
  • fuzion_reaktor
    fuzion_reaktor over 12 years ago in reply to kidiccurus +1
    Motors, yes are a plugging in problem. This is just weird. But switching the two works and I have successfully printed a small misshaped cube...Progress...
Parents
  • D_Hersey
    0 D_Hersey over 12 years ago

    'Chopper drive' means a current-source drive that is swichmode.  The CS driver is intended to minimize the effect of coil inductance.  Your motor coil has resistance and inductive reactance.  The coil is ill-wont to allow changes in the current going through it.  It sources its own potential to oppose attempts to change this current.  Current source drive introduces a super voltage during the initial moment to overcome (establish the new magnetic field) the reactive component of the load more quickly.  CS drivers are less sensitive to loading vagaries.

     

    Stepper motors at rest detent at the full steps.  If the rotor is intended to remain at rest in a micro-step, the ratio of the currents in the coils have to be maintained, but they can be mutually diminished.  This is the other side of chopper drive.

     

    It is sorta fun to adjust the current from an insufficient to a tenable range.  The motor clicks helplessly then get's it together, it's rather like watching a toddler rise from the floor.

     

    There was an interesting developmental pathway to these apotheosis off-the-shelf CS-chopper drives, which will soon, properly be lost to history.  In the early days, an external resistor was associated with each coil and the potential souped-up.  A common setup with industrial-grade printers was a 12V driving a 5V stepping motor with resistors 7/5s as large as the motor coil resistances.  The next step (neglecting nxQ schemes) was activating (cascode) the loads, but it took awhile to develop a current source circuit that was both modulatable and fast.  I've drawn the circuit that broke the logjam in another post.  Kids today!  You don't know how good ya' got it!

     

    I should note that, even if you just drive your motors detent-to-detent 'micro-stepping' is really sweet because it takes lotsa unwanted high-derivative mechanical energy from the system as regards square-wave drive.  The motor runs quieter, everything is smoother, less whiny.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ootbrobo
    0 ootbrobo over 12 years ago in reply to D_Hersey

    More about the relationship of micro-stepping and torque capability

    http://www.micromo.com/microstepping-myths-and-realities

     

    More about the relationship of speed vs torque

    Speed - Torque Curves for Stepper Motors

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ootbrobo
    0 ootbrobo over 12 years ago in reply to D_Hersey

    More about the relationship of micro-stepping and torque capability

    http://www.micromo.com/microstepping-myths-and-realities

     

    More about the relationship of speed vs torque

    Speed - Torque Curves for Stepper Motors