element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How Do You Solder without Flux?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 31 subscribers
  • Views 6118 views
  • Users 0 members are here
  • soldering
Related

How Do You Solder without Flux?

e14 Contributor
e14 Contributor over 12 years ago

How do you solder without flux?  I see people do it and the solder connections look solid and shiny.  I know that using leaded solder makes it easier, but I still need to use flux in order to get that solid and shiny connection.  I've heard that using solder with a particular ratio of flux to solder is important.

  • Sign in to reply
  • Cancel
Parents
  • jw0752
    0 jw0752 over 12 years ago

    Hi Paul,  Jbix was corect to point out the need for clean metal. I often will wire brush or use fine sand paper if the wires or traces to be soldered look dull. Your solder iron heat, if it is indeed 800 degrees is too hot. At this temperature the rosin will boil away and the solder will oxidize quickly. Do you get a puff of smoke when you apply the solder to the iron? If you do it is probably too hot. A more appropriate temperature is between 600 F and 700F. According to the solder manufacturers there is a shelf life to solder though I have used rosin core solder 20 years old without too much problem.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jw0752
    0 jw0752 over 12 years ago

    Hi Paul,  Jbix was corect to point out the need for clean metal. I often will wire brush or use fine sand paper if the wires or traces to be soldered look dull. Your solder iron heat, if it is indeed 800 degrees is too hot. At this temperature the rosin will boil away and the solder will oxidize quickly. Do you get a puff of smoke when you apply the solder to the iron? If you do it is probably too hot. A more appropriate temperature is between 600 F and 700F. According to the solder manufacturers there is a shelf life to solder though I have used rosin core solder 20 years old without too much problem.

    John