element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum How Do You Solder without Flux?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 31 subscribers
  • Views 5990 views
  • Users 0 members are here
  • soldering
Related

How Do You Solder without Flux?

e14 Contributor
e14 Contributor over 12 years ago

How do you solder without flux?  I see people do it and the solder connections look solid and shiny.  I know that using leaded solder makes it easier, but I still need to use flux in order to get that solid and shiny connection.  I've heard that using solder with a particular ratio of flux to solder is important.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thanks so much.  So I've learned that, even though the manufacturer shows a shelf life of 2 years, that may not be a big concern.  Also, that for leaded solder, my iron temperature should be between 600F and 700F.  I do see smoke when I solder which substantiates that 800F is too darn hot. I learned from the Kester website that there are variety of cored solder with a variety of types of chemical.

     

    I think I will lower my iron to 700F and see what happens.

     

    Thanks again.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • michaelwylie
    0 michaelwylie over 12 years ago in reply to e14 Contributor

    I'm interested to see if the reduction in temperature solves your problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelwylie

    Yes, absolutely (said with a huge smile on my face)!!!  I only changed the tip from 800F to 600F and it worked great.  There was only a little smoke when I added the solder to the joint and no sputtering like it did before.  The solder just melted and spread like it should.  I now make sure I tip the tip after each use.

     

    I think I do want to try solder with different flux in the core. I'm wondering if there is a solderability trade-off if I use a no-clean solder.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to michaelwylie

    Yes, absolutely (said with a huge smile on my face)!!!  I only changed the tip from 800F to 600F and it worked great.  There was only a little smoke when I added the solder to the joint and no sputtering like it did before.  The solder just melted and spread like it should.  I now make sure I tip the tip after each use.

     

    I think I do want to try solder with different flux in the core. I'm wondering if there is a solderability trade-off if I use a no-clean solder.