element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Try to modify regular printer to print PCBs
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 33 subscribers
  • Views 1739 views
  • Users 0 members are here
  • build_challenge
Related

Try to modify regular printer to print PCBs

e14 Contributor
e14 Contributor over 12 years ago

Try to modify regular printer to print PCBs on that copper boards.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The Epson printer is a neat idea, I was wondering if a DVD-W Laser diode would have enough power to burn off the paint like Ben does with the laser cuter. Then it could be as simple as using one in place of the jhead of a 3d printer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The Epson printer is a neat idea, I was wondering if a DVD-W Laser diode would have enough power to burn off the paint like Ben does with the laser cuter. Then it could be as simple as using one in place of the jhead of a 3d printer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mysticmindset
    0 mysticmindset over 12 years ago in reply to e14 Contributor

    The dvd-w laser is something i thought of also. I took the diode out. I took apart a laser pointer flashlight combo and put the lens up to the laser with my hands. I was able to burn electrical tape, visible draw lines on the black plastic cover for the cd tray, burn lines on a wooden ruler, burn lines on calluses and scar on my had(kinda smelled bad:-) ), melt black powder coating together, but would not make a mark on a piece of metal that was from what i assume painted black from an old flat bed scanner i took apart. Also it would not burn paper. I bought a voltage regulator and in the mix of trying to get the correct voltage i believe i burnt up the laser diode and have not messed around with it since. After i put the lens and diode together with my hands and it got hot i milled a heat sink/ mount for the diode and lens so i could put it on a gantry system i was going to make out of old okidata dot matrix printer slides and stepper motors. I got into trying to look up the motor controller chips on old cd rom control boards to see if they could take direction and pulse commands for easy integration with arduino and cnc control software as they obviously control stepper motors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mysticmindset

    Anthony,

     

    There is info on power requirements and how to use them at Laser diodes from CD-RW drives can cut and burn!

    They are 5.6mm and you can buy housings/heat sinks on ebay for $3-$5 with lenses.

     

    Seems like it would be an easy mod and very useful, once I get my 3d printer built ill have to look into playing with one.