element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Try to modify regular printer to print PCBs
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 33 subscribers
  • Views 1752 views
  • Users 0 members are here
  • build_challenge
Related

Try to modify regular printer to print PCBs

e14 Contributor
e14 Contributor over 12 years ago

Try to modify regular printer to print PCBs on that copper boards.

  • Sign in to reply
  • Cancel
  • vinceverc
    0 vinceverc over 12 years ago

    That would be cool.

    But can you be a bit more specific?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to vinceverc

    So he can took it apart and modify use paper  feeders to feed printer with blank PCBs and fill cartridges with ink that can be removed by water and can`t be removed by etching. Sorry about grammer if it isn`t correct.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • toxxn
    0 toxxn over 12 years ago in reply to e14 Contributor

    I believe what the idea here is, to modify a laser ink jet printer to print directly on copper clad, in turn creating a PCB Printer.

    The printed board would then need to go through a treatment process using an etching liquid such as Ferric Chloride or CCiAHAS.

    (Copper Chloride in Aqueous Hydrochloric Acid Solution. A solution for those who are more environmental or simply don't know how to dispose of Copper Chloride, the left behind solution after etching using Ferric Chloride. Can be re-used indefinitely as well.)

    And then of course the final step of drilling your holes, unless otherwise a surface mount board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to toxxn

    I thought to use  ink printer becuse it can be very compact and you dont need to buy new cartridges. So you can use your old printer cartridges and drill hole on top of cartridge fill it with that special ink and just  modify feeders for paper to feed copper PCBs. If you want to make more PCBs you will use biger blank PCB but if you want one small PCB that is the problem it is too small to feed I just realize now so it will be better to use some kind of plate to move blank PCBs somethink like this sorry about useing  paint but I was thinking that  it will be great mechanical and electrical modifying fo Ben Heck

     

    this will be grat mechanical an electimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • toxxn
    0 toxxn over 12 years ago in reply to e14 Contributor

    Actually using paint or a similar program is a great way to quickly show a sketch or diagram.

     

    I think this project wouldn't be very complicated and quite doable, however I think the main problem is the ink. The ink used would have to be an acrylic ink and I am unsure of how well the print would come out. That is to say, I am unfamiliar with acrylic inks other than acrylic pens specifically used for PCB's, which could be used in a CNC type PCB printer although a whole different project on it's own.

     

    As for the size of the PCB, if you were not interested in a large batch of PCB's at once, a solution other than a jig as you explained above would be to modify a smaller printer alongside a larger one. The great thing about this idea, there are so many different sized printers out there, even portable ones.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to toxxn

    Maybe not you need to make a case to fit all components. And if the feeders are steper motors just relocate and put some gears and teeth on plate and just use old software. This project is all about reloceting old components and puting some new parts. And yes most difficult part fill be ink I will be happy if Ben Heck will do that project.

    And thanks for advices.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • toxxn
    0 toxxn over 12 years ago in reply to e14 Contributor

    No problem.

    Glad to be of some assistance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 12 years ago in reply to e14 Contributor

    Directly printing to copper is very tricky and expensive. Luckily Ben has something to do it accurately, a laser cutter. More specifically he applys a layer of black spray paint and uses a laser cutter to burn it away. You can make a laser from a printer so perhaps this is a better project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mysticmindset
    0 mysticmindset over 12 years ago

    This has already been done. If you search epson pcb printer mod it comes right up. I have been researching ways of making pcb's and have read thru it. He hacks the printer to raise the print head and uses a plate to hold the pcb for more accurate feed. Some epson printers have a lever for raising and lowering the print head. The epson uses a different print head, a micro-pezio for using pigmented ink. Read all about it i have been scouring thrift shops for an epson and just waiting to find one i want to do this to.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The Epson printer is a neat idea, I was wondering if a DVD-W Laser diode would have enough power to burn off the paint like Ben does with the laser cuter. Then it could be as simple as using one in place of the jhead of a 3d printer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>