element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Metal Detector using hall effect sensor
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 33 subscribers
  • Views 4111 views
  • Users 0 members are here
  • detector
  • effect
  • metal
  • hall
  • sensor
Related

Metal Detector using hall effect sensor

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

I want to build a metal detector through a hall effect sensor. This detector will be a rectangular tube design hollow from inside and multiple hall effect sensors will be arranged along the length of the tube in the inner walls. Now when a metal object passes through the tube, theses sensors should be able to tell about it. The whole idea is to utilize the variations in the earth's magnetic field inside the tube when metal object passes through and sensors will pick up this little variation to detect metal.

 

Now, I know this could be difficult with hall effect sensor. The variation in the earth's magnetic field will be too little for the sensor to detect it. However, there could be some way of getting this done. One way could be to magnetize the path inside the rectangular tube, so a passing by metal object gets magnetized and induce greater variations in the field.

 

Could you recommend some other possibilities of doing this. Some solution, that will give very reliable detection, zero false alarm and better range of detection so that the size of rectangular tube could be actually increased, making this design practical ?

 

I would look forward to the suggestions of you guys. Kindly reply

 

Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • D_Hersey
    D_Hersey over 11 years ago +1
    You can use a permanent magnet on one side of the tube with your detector on the other and try to detect diminutions in the magnetic field as ferrous material flows by, soaking up some of the PM's magnetic…
  • DAB
    DAB over 11 years ago +1
    I am not sure that you can get a sensitive enough reading using the hall effect sensor. Have you looked at the TI LDC board? It is very sensitive to magnetic fields. Also, some metals are diamagnetic,…
Parents
  • DAB
    0 DAB over 11 years ago

    I am not sure that you can get a sensitive enough reading using the hall effect sensor.

     

    Have you looked at the TI LDC board?  It is very sensitive to magnetic fields.

     

    Also, some metals are diamagnetic, which means that they behave differently to magnetic fields than conductive metals.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DAB
    0 DAB over 11 years ago

    I am not sure that you can get a sensitive enough reading using the hall effect sensor.

     

    Have you looked at the TI LDC board?  It is very sensitive to magnetic fields.

     

    Also, some metals are diamagnetic, which means that they behave differently to magnetic fields than conductive metals.

     

    DAB