element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Single Drive Multi Console
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 1 reply
  • Answers 1 answer
  • Subscribers 29 subscribers
  • Views 355 views
  • Users 0 members are here
Related

Single Drive Multi Console

e14 Contributor
e14 Contributor over 11 years ago

So I've recently rebuilt an arcade machine which introduced me into all sorts of aspects of electronics I haven't dealt with before. While working on it and watching the Ben Heck Show, I had an idea but don't know if I'm looking at the impossible.

 

Ben did a build of an X360, PS3, and WiiU all in one box a while back, but with the new consoles out all of them use BluRay (XBone and PS4 at least, I haven't checked WiiU) or a BluRay equivalent (as the two listed can play bluray movies). Would it then in theory be possible to combine the two consoles into one, but use just a single BluRay drive from one of them to to go both? Possibly bulid some interface that detects the game put in and boots the correct system even?

 

I realize this could probably be a nightmare if possible, but the question is if this is even possible to begin with or is there something I am unaware of?

  • Sign in to reply
  • Cancel
  • jlcarender
    0 jlcarender over 11 years ago

    I am not sure about the current systems but I do know that the drives for the xbox360 and the ps3 are hard coded for each system. and neither one can be used on the other system. and there is no reason why the xbox one and ps4 would not be configured the same way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer