element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Refrigerator Oven
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 30 subscribers
  • Views 399 views
  • Users 0 members are here
Related

Refrigerator Oven

e14 Contributor
e14 Contributor over 11 years ago

Hi, a long time ago I heard of an oven that would double as a refrigerator. The idea was to keep a meal cold until one was ready to go home at which time they could send maybe an Email to it and start cooking their food. Like I said this was some time ago but I have yet to see one on the market. Does anyone think it would be possible to build something like this?  

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 11 years ago

    The Polara range of ovens from Whirlpool combines the two most incompatible kitchen appliances - it's an oven that acts like a fridge. The unique oven allows you to prepare a dish, place it in the oven where it keeps cool all day to begin cooking at a pre-programmed time so that dinner's ready when you get home. Polara will even switch back to refrigeration if you arrive home late. 

    The cooking capabilities of the Istandard-sized 30-inch Polara range include a convection system that delivers up to 30% faster cooking times and it will keep food cool for up to 24 hours before it begis cooking. Available in Black, Pure Biscuit, Pure White and Stainless Steel for US$1799-$1899. No word as yet on an Australian release.

    from http://www.gizmag.com/go/1524/

     

    Apparently nice idea but too expensive to sell many at that price.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kidiccurus
    0 kidiccurus over 11 years ago in reply to clem57

    If you need to make something like this then a peltier modual might be a good start. If you use a h-bridge to change the direction of the current, you can use the same modual to both heat and cool the food. The main issue would be the maximum temperature, I don't think it is safe to bring a peltier over a certain temperature this oven may have to reheat previously cooked food rather than freshly cooking the food.