element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Replacing the battery in a 2600 mAh power bank
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 30 subscribers
  • Views 905 views
  • Users 0 members are here
Related

Replacing the battery in a 2600 mAh power bank

e14 Contributor
e14 Contributor over 11 years ago

I have this power bank but the 2600 mAh capacity isn't enough for my needs. I've got 4 spare 18650 Li-on batteries and I was wondering if I could connect them up to the original circuit in parallel? Here are a few photos of the power bank as it is:

image

 

imageimage
  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 11 years ago

    willp789

    Let us begin with 2600 mAh which is 2600 mAmperes the battery delivers per hour. If this is a typical USB like in the picture, I would guess the battery is a 3.7 Lipo. The circuit on the USB converts from 3.7V to 5V which lowers the amperes. Based on the assumption, 2600 mAh x 3.7 V = 9.6 WH

    Product DetailsIs this what you have?

     

    These are 5000mAh. So one cell is also 3.7v and now you have 5000 mAhx3.7 V = 18.5 WH which is double the draw. Bottom line is yes if they are both same volts and the USB circuit does what I surmise is true. Just make sure to get the wiring correct!

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Yes, all the batteries are in the region of 3.7v but I will start by charging each of the batteries individually to full with the circuit before I connect them all together.

    Thanks for your help Clem!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to e14 Contributor

    Glad to here. It helps me if you mark my answer as correct after you try this. Thanks.