element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum 10NES Chip Help!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 32 subscribers
  • Views 1388 views
  • Users 0 members are here
  • nes
Related

10NES Chip Help!

jnrz81
jnrz81 over 11 years ago

Hi. I'm not sure if this is the right place to post this, but I'd appreciate the help.

 

I disabled the 10NES chip in my NES and it no longer blinks. But now I only get a green screen, whether there's a game in it or not. Help! What do I do?

  • Sign in to reply
  • Cancel
Parents
  • jnrz81
    0 jnrz81 over 11 years ago

    I only removed the 4th pin. And yes, it doesn't blink anymore like it used to. But now I only get a green screen! Games no longer play. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kennyl
    0 kennyl over 11 years ago in reply to jnrz81

    http://www.raphnet.net/electronique/nes_mod/nes_mod_en.php

    "All you need to do is put both chips in key mode. When both lockout chips are in key mode, nothing happens (so no resets). To do this, you must disconnect lockout chip pin 4 from the motherboard and connect it to a ground (lockout chip pin 11,12,13,14 or 15). It will also work if pin 4 is not connected at all, so don't worry if you accidentally rip it off. Even though it works without connection pin 4 to ground, I believe it is better to do it anyway."

     

    Sounds like you "shouldn't" have to ground after doing this, but it might not hurt.  Also, connectors cause all kinds of issues if you're using the NES-001 front loader.  If you didn't clean the NES motherboard connector (the one the 72 pin slips over) I'd break it back down and do that as well as clean all of your games.  The best way to clean the games is to use the special bit or make one as on the website above, though I personally had little luck with making one.  They are fairly cheap to buy on eBay or various websites.  Once you get the cartridge apart, it can be cleaned with a simple rubber eraser like those used to remove pencil marks.  Also, 72 pins are relatively cheap to replace if you're doing it yourself but you can follow the guides to "restore" them as in the website above.

     

    Here is a video I made on the "take apart/eraser" method of cartridge cleaning that actually displays me cleaning a game and shows the difference in real time.  My before/after comparison was broken by the fact I tested a cart at first that was assembled with flat-blade screws and I then had to improvise on camera since I didn't have my flat blade screwdriver handy.  FYI, both games failed to work before cleaning and then did work afterwards so this method is a possible fix.  Some early NES carts left the factory with the flat blade screws (and you'll notice they are usually are held by 5 screws instead of 3), but they developed the "tamper resistant" screws fairly quickly after that so 90% of NES games you'll find use them.  https://youtu.be/Y9UmcEVJMPM

     

    Try the pin restoration, NES motherboard edge connector cleaning (the pins which the 72 pin connects to inside the NES), and game cart edge cleaning first in my opinion.  The lockout chip really should only have to be cut on pin 4, but you might ground it for a check.  Just be sure to not short anything that shouldn't be shorted. image  Using these tricks, I've never seen any condition NES fail to load games, including badly yellowed/physically damaged/child abused consoles.  They just rarely die to the point where they can't be fixed, they're incredibly reliable.  Clean games taken into account, actual NES console problems only reside with the lockout chip 1% of the time and with the 72 pin about 99% of the time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kennyl
    0 kennyl over 11 years ago in reply to jnrz81

    http://www.raphnet.net/electronique/nes_mod/nes_mod_en.php

    "All you need to do is put both chips in key mode. When both lockout chips are in key mode, nothing happens (so no resets). To do this, you must disconnect lockout chip pin 4 from the motherboard and connect it to a ground (lockout chip pin 11,12,13,14 or 15). It will also work if pin 4 is not connected at all, so don't worry if you accidentally rip it off. Even though it works without connection pin 4 to ground, I believe it is better to do it anyway."

     

    Sounds like you "shouldn't" have to ground after doing this, but it might not hurt.  Also, connectors cause all kinds of issues if you're using the NES-001 front loader.  If you didn't clean the NES motherboard connector (the one the 72 pin slips over) I'd break it back down and do that as well as clean all of your games.  The best way to clean the games is to use the special bit or make one as on the website above, though I personally had little luck with making one.  They are fairly cheap to buy on eBay or various websites.  Once you get the cartridge apart, it can be cleaned with a simple rubber eraser like those used to remove pencil marks.  Also, 72 pins are relatively cheap to replace if you're doing it yourself but you can follow the guides to "restore" them as in the website above.

     

    Here is a video I made on the "take apart/eraser" method of cartridge cleaning that actually displays me cleaning a game and shows the difference in real time.  My before/after comparison was broken by the fact I tested a cart at first that was assembled with flat-blade screws and I then had to improvise on camera since I didn't have my flat blade screwdriver handy.  FYI, both games failed to work before cleaning and then did work afterwards so this method is a possible fix.  Some early NES carts left the factory with the flat blade screws (and you'll notice they are usually are held by 5 screws instead of 3), but they developed the "tamper resistant" screws fairly quickly after that so 90% of NES games you'll find use them.  https://youtu.be/Y9UmcEVJMPM

     

    Try the pin restoration, NES motherboard edge connector cleaning (the pins which the 72 pin connects to inside the NES), and game cart edge cleaning first in my opinion.  The lockout chip really should only have to be cut on pin 4, but you might ground it for a check.  Just be sure to not short anything that shouldn't be shorted. image  Using these tricks, I've never seen any condition NES fail to load games, including badly yellowed/physically damaged/child abused consoles.  They just rarely die to the point where they can't be fixed, they're incredibly reliable.  Clean games taken into account, actual NES console problems only reside with the lockout chip 1% of the time and with the 72 pin about 99% of the time.