element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum Relay trouble with ATX power supply
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 16 replies
  • Subscribers 33 subscribers
  • Views 3374 views
  • Users 0 members are here
  • halogen
  • 12v
  • arduino nano
  • power supply
  • relays
  • atx
  • beginners
  • electronics.
  • arduino
  • novice
  • beginner
Related

Relay trouble with ATX power supply

dukeofmarshall
dukeofmarshall over 10 years ago

Full disclosure: I'm a beginner electronics enthusiast. Here is my setup:

 

(1) Arduino Nano

(1) Arduino 24v 3 amp Relay Shield

(1) MR5A001A1 12v 30 amp Relay from an Isuzu Rodeo

(1) ATX Power Supply Model ATX-1956D

(1) 12v 50w Halogen Light Bulb

 

So the end goal is to drive the halogen bulb with the Arduino. Be able to turn it on and off as needed. For my first setup, I connected the Arduino to the relay shield, ran a 12v line from the power supply unit to the common on the relay, and the NO from the relay to the halogen bulb. I did not take the amps of the bulb into account at first but soon realized my mistake when the relay fried. I replaced the Arduino relay and the PSU just to be sure and added the car relay. My current setup is Arduino Nano connected to the Arduino relay, one 12v line from the PSU is connected to the common on the Arduino relay, the NO on the Arduino relay is connected to the trigger(?) of the car relay, one 12v line from the PSU is connected to the common on the car relay, and the bulb is then connected to the NO of the car relay. The Arduino and the Arduino relay shield are both powered from a 5v line from the PSU.

 

The issue I'm having is when the Arduino relay switches on and turns on the car relay, the PSU just shuts down. Now, I can power the bulb directly with the PSU, no problem. But when connected up in this setup something's causing the PSU to shut off. Strangely enough, If I connect the bulb to the NC of the car relay, the bulb powers up with no problem. Then, as expected, when the Arduino relay switches on the car relay, the bulb goes off, but when the Arduino relay switches off and turns off the car relay, activating the NC of the car relay again, the PSU immediately shuts down like before.

 

Anyone have any ideas or suggestions about this? All the parts seem to be in order. There's not too much voltage going into any part and, now, all the parts should be able to handle the amperage with the PSU being more than enough to power the whole system. What am I missing here?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 10 years ago +3
    Incandescent light bulbs, including halogen types have a very low resistance when first powered up. It can take hundreds of milliseconds before they warm up to white hot and at that point their resistance…
  • jw0752
    jw0752 over 10 years ago in reply to dukeofmarshall +3
    Hi Todd, Sorry it took so long to get back to you. One thing that you might try is to use an In-Rush Thermistor in series with the bulb. I discussed these Thermistors a while back in a previous blog. https…
  • shabaz
    shabaz over 10 years ago +2
    Hi Todd, According to this ePanorama.net - Links (bottom half of that page) such PC power supplies need a certain load on their 5V rail too. It is an unexpected situation that there is a heavy load on…
Parents
  • D_Hersey
    D_Hersey over 10 years ago

    Depends what you are going for.  Halogen emission is more like blackbody radiation.  LEDs are typically fairly narrow in their emission spectrum.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 10 years ago

    Depends what you are going for.  Halogen emission is more like blackbody radiation.  LEDs are typically fairly narrow in their emission spectrum.