element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Forum LM317/LM338 Current Limit Mode
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 31 subscribers
  • Views 1010 views
  • Users 0 members are here
Related

LM317/LM338 Current Limit Mode

flaredelectronics
flaredelectronics over 9 years ago

This should be pretty simple, but I want a clear answer before I assume and continue.

 

LM317/LM338 has two popular modes, Voltage Regulation (Positive), and Current Regulation(Negative)

317 = ~1.5A 338 = 5A

 

My question is, when in current limit mode, is the current sourced from the Middle Pin or the Adjust Pin.

 

The reason to ask is, between the middle pin and sense pin you put the resistance, but I want to know if all the current is sourced from the middle pin.

Specifically, if you want to source 5A from the 338, do you need a resistor capable of 5A. (Example 5v 5v R1=25W)

 

I am curious if it is feedback only or if you really must have a resistor capable of passing 100% current.

 

 

 

 

 

 

Extra Information:

Once I know, I am going to use a PTC/NTC or IRCL in place of the resistor. (ICL = 2.2ohm 3.7A max)

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 9 years ago +2
    Hi Keith, Yes your sense resistor must be able to handle the current which is supplied by the center output pin. As Don D_Hersey stated the LM 317 has a 1.25 Volt difference between Vout and Adjust. If…
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi Keith,

     

    Yes your sense resistor must be able to handle the current which is supplied by the center output pin. As Don D_Hersey  stated the LM 317 has a 1.25 Volt difference between Vout and Adjust. If you use a 1.25 Ohm resistor for the sense your 317 will be a 1 Amp current source. (1.25 V / 1.25 Ohms = 1 Amp)  If the Sense resistor is 5 Ohms your current source will be regulating at 250 mA. (1.25 V / 5 Ohms = 0.25A). Since the sense resistor will always have 1.25 volts across it you will need a wattage rating that matches or exceeds the current you are regulating times 1.25 Volts. Don indicates that this would be 6 watts in the case of a 5 A current source and your sense resistor in this case would have to be 0.25 Ohms. ( 1.25 / 0.25 Ohms = 5 A)

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 9 years ago

    Hi Keith,

     

    Yes your sense resistor must be able to handle the current which is supplied by the center output pin. As Don D_Hersey  stated the LM 317 has a 1.25 Volt difference between Vout and Adjust. If you use a 1.25 Ohm resistor for the sense your 317 will be a 1 Amp current source. (1.25 V / 1.25 Ohms = 1 Amp)  If the Sense resistor is 5 Ohms your current source will be regulating at 250 mA. (1.25 V / 5 Ohms = 0.25A). Since the sense resistor will always have 1.25 volts across it you will need a wattage rating that matches or exceeds the current you are regulating times 1.25 Volts. Don indicates that this would be 6 watts in the case of a 5 A current source and your sense resistor in this case would have to be 0.25 Ohms. ( 1.25 / 0.25 Ohms = 5 A)

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • D_Hersey
    D_Hersey over 9 years ago in reply to jw0752

    If you put a protection diode on each line, probably a shottky, you can parallel VRs in current source mode, IIRC.