Hack Like Heck
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Hack Like Heck
  • More
  • Cancel
Hack Like Heck
Blog Nobble's RetroPie Futureboy DMG RPi3 Handheld (ENTRY BLOG 4 HACK LIKE HECK)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Hack Like Heck to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: nobble
  • Date Created: 8 Mar 2018 12:37 PM Date Created
  • Views 4210 views
  • Likes 5 likes
  • Comments 20 comments
  • sudomod
  • pi 3
  • portable
  • nobble
  • hdmi
  • ben heck show
  • ben heck
  • neopixel
  • bitbuilt
  • raspberry pi
  • thefuture
  • gameboy zero
  • pico projector
  • touchscreen
  • hack like heck
  • handheld
  • arduino
  • dmg
  • hlhblog
  • video games
Related
Recommended

Nobble's RetroPie Futureboy DMG RPi3 Handheld (ENTRY BLOG 4 HACK LIKE HECK)

nobble
nobble
8 Mar 2018

image

NOBBLE HAS STEPPED UP TO THE CHALLENGE!
( ͠° ͜ʖ ͡°)


Alright folks, benheck doesn't give a hack anymore. image

 

Now is the time for us in the modding community to RISE UP by blowing the minds of unknowingly innocent normies with our next level mods.

 

Luckily, I woke up to the notification the morning of the contest video, and without even brushing my teeth I got my camera out to film My Audition!

 

I was the first person to enter and have been getting nothing but joy and thrill out of this contest so far!

 

Thanks for all the support everyone!

 

I want to take a moment to thank a few individuals before going into detail of my build.

 

  • Ben Heck & Team - You are one smart cookie! I want to thank you for piquing my interest in electronics modding at such an early age. You helped me find a community that is very humble and appreciative of all the information and work done in Portablizing consoles. Thanks to Felix, Karen, and everyone else involved with the show and this contest!!!
  • Kitschbent LLC - For being my Official Sponsor for the contest and providing me with the Gameboy Shell and other items from your shop to help with my build! You are a great source for custom Gameboy parts. I really appreciate your interest and trust in my abilities!
  • Spencer Richardson - Thank you for helping me 3D print the parts needed for my build! I really appreciate going the extra mile for me! Spencer makes really cool 3D printed night lamps that are for sale in his Etsy Shop
  • ShockSlayer - Bro, you are ridiculously supportive and such a great meme. When ModRetro was blooming, you were such help and a big inspiration to my builds starting out when I was only a kid. Thanks for all the help getting me back into the community when I was just a lost piggy in the big city. I am glad to be here with everyone.
  • Madmorda - I really am glad to see others from the BitBuilt Forums really engaged in this contest and ready to mod! Good luck, your abilities are Crystal Clear, ShockSlayer can concur! Thanks for your support!
  • Fibbef - For help with a special scene in my video! Thank you so much for all your time and effort! You rock!!!
  • Portablizers, & Everyone else in the Community - Everyone who mods, matters. Lately I have gotten closer to a few of you fine individuals online and I want to thank YOU ALL for the support, help, friendly banter, amazing creations, and the gained insight from that to Be Excellent To Each Other.... AND PARTY ON DUDES!  VOTE FOR NOBBLE!

Alright! Moving forward..

 


My entry build is Officially Titled: Nobble's RetroPie Futureboy

image

It is a portable emulation handheld resembling the well-known Gameboy with features NEVER BEFORE SEEN BY MANKIND! I have been time traveling to the past to find the source of Portable Video Game Consoles, as well as going further beyond into the future, learning how to hone modern technology in ways only dreamed of! I've based this on the Raspberry Pi 3, running a custom version of RetroPie from tweaks I made, and loaded with extra features!

 

Case: The handheld case is a custom mold for a Nintendo Gameboy DMG made by Kitschbent. I will be modifying the insides to make it more roomy for the components.

 

Main board: I am using an almost fully stock Raspberry Pi 3 that will have a hat screen attached on top. The only modifications I will do is removing one set of USB ports for hard wiring components.

 

Screen(s): I am using a 3.5" HDMI touchscreen "hat" for main display. GPIO will control the touchscreen panel. ON TOP OF THAT I am adding in a pico projector you can switch to, that will illuminate gameplay onto any surface of your choosing. That will be housed inside a Shark MX cartridge made by GameShark. It was a modem cartridge for internet access and email on the gameboy. Service was called GB-Mail. I'm sure it was indeed terrible.. CUE THE MEMES.


Controls:
I will be using an Arduino Pro Micro that will be setup as a USB gamepad with a layout seen commonly on most controllers these days. Dual Analog thumbsticks and dual triggers along with the usual d-pad and ABXY, Start, Select. I need a few 3D printed parts to install the button wells and button supports with ease. *Thanks Spencer!


Audio:
The goal is to have a working stereo audio Amp connected to the Pi so that when I insert headphones into the jack, the audio cuts out and goes to headphone line. I may end up going with mono, time will tell.

 

Batteries/Power: I am using a 3.7v 7000mah Li-Po cell that will be connected to a portable battery bank BCM PCB to regulate power @ 5v 2.1A to power everything. Charge port will be a Micro USB jack, and battery life is expected to be around 3-6 hours.


Other Modifications & Features:
I will be adding Programmable NeoPixel RGB LEDs all over inside the case so you can hail a UFO from space. What is a Futureboy without some new age colorful tech? I will be either programming them from the Pi itself, or Arduino. I also have a silicone cover to finish off the build aesthetically. It slides snugly right over the case for added protection.

 

Check out my Instagram for all pictures and video clip samples on this project! I will update frequently!

 

Edit: March 30, 2018 (Only a few days remain! THANK GLOB!!!)

 

Okay, the contest is coming to an end and I have been HACKING LIKE HECK to finish this up! I am in the home stretch, and though this work log is lacking frequent updates, you can follow me on Instagram for daily posts.

 

Also check out my GOOGLE DRIVE FOLDER with tons of pics and video clips from this build!

 

DMG Case Demo w/ Neopixels

 

Just look at how awesome Matt Kitschbent's custom clear DMG case looks with neopixels inside illuminating it!

 

I am almost done getting everything wired up and securely fit inside the case. I had a little snafu with Amazon, but after many hours with customer service I am finally getting the last parts I ordered 2-day shipping and still aren't in hand. I have wasted a few days with this and have been editing my video in the meantime. But I did order a new soldering iron since I seemed to have ruined all of my tips during this hasty build! A brand new TS100 is soon to be mine!

 

The final video is due April 2nd. I have much faith in this entry and feel it a top 10 prize winning project for sure! The video will testify.. #hack2thefuture #futureboy

 

I hope I can get the support from the people of this site and the community of all makers, modders, hackers, DIY-enthuseists alike to help vote for my entry upon time. I have had so much help and support so far from the community, and my official sponsor Kitschbent LLC. It's been lots of fun! image

 

Anyways, thanks for checking out my build entry! I hope you enjoy what is to come of THE FUTURE (BOY)!!!

      VOTE HERE!

image

  • Sign in to reply

Top Comments

  • nobble
    nobble over 8 years ago in reply to rocits +3
    That was my thought exactly with AR and VR so heavily flooded in our society today. Screens are so obsolete. Check out this review, it might give you some in-SIGHT as to what my plans are. www.youtube…
  • nobble
    nobble over 8 years ago in reply to rocits +2
    I love MGB handhelds! They are my favorite gameboy. I've backlight modded and biverted quite of few of those in the past. I actually have a tutorial almost complete I need to upload to YouTube. I should…
  • nobble
    nobble over 8 years ago +2
    UPDATES! COLORFUL ONES! I am almost done! The clock is ticking. I wonder how many more sleepless nights I will endure to finish this up!?!?! Time4Miracles.
Parents
  • rocits
    rocits over 8 years ago

    How's it going Nobble? Hope you're freakin' sleepin' dude! =D You'll be really glad of the 4/4 'sleep extension' then! lol  loads of top peeps are out exhausted/fails , it seems, freaky stuff!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rocits
    rocits over 8 years ago

    How's it going Nobble? Hope you're freakin' sleepin' dude! =D You'll be really glad of the 4/4 'sleep extension' then! lol  loads of top peeps are out exhausted/fails , it seems, freaky stuff!