Community Feedback
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Community Feedback
  • More
  • Cancel
Community Feedback
Forum Basic Electronic Queries
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Feedback to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 3 answers
  • Subscribers 7 subscribers
  • Views 1572 views
  • Users 0 members are here
Related

Basic Electronic Queries

e14 Contributor
e14 Contributor over 10 years ago

Hi,I had following queries :

1.Are 1602 and 16*2 just different names for same LCD module?

2.How  to identify whether the cheap LCD modules has HD44780 controller board inbuilt?

3. While operating DC brushed motor if it is specified 5v-9v ,what is safe operational voltage? 4. While operating DC brushed motor how to calculate amperage rating to prevent frying out power supply?

5.Which are best type of DC motor for attaching drill bits?

Awaiting for reply! Thank you!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +3 suggested
    Just to add some more useful info on the LCD's - you can often buy them with an i2c backpack which can simplify their usage and reduce the amount of wires to connect to them considerably, by buying one…
Parents
  • jw0752
    0 jw0752 over 10 years ago

    Hi Apoorva,

    I do not know the answer to your question on the LCD module but I will tell you what I know about the motor question.

     

    If the motor is rated for 5v to 9v this means that the motor will turn dependably at 5 volts and at 9 volts it will be at its full duty cycle voltage. More than 9 volts can be applied for short periods of time but the motor may spin faster than it is designed for when under no load. The current draw of the motor under any specific voltage will increase as load is applied to the motor. For example if we have a motor drawing 1 amp at 9 volts with no load and we make the motor spin a drill bit that is boring so that the drill bit slows the motor the current will increase. We could see the amperage go to 2 amps, 3 amps and so on as more load is applied to the motor. Ultimately too much load will stall the motor and we will get a stall current. This will quickly overheat and burn the windings in the motor. Your power supply will likely have a limit to the current that it can supply. This may prevent damage to the motor but it will also limit the power you can get out of the motor.

     

    Very few motors that I know of are designed to have drill bits attached directly. In most cases the motors are geared down so that the drill bit turns at a slower speed but has a lot more torque. This is of course exactly what is done in a battery powered hand drill. I do not know what you are building but will a battery powered hand drill work. You would have a DC motor and a drill chuck.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jw0752

    Thank you John for your detailed answer!

    I was thinking of making drill with USB power supply(5v)

    There are videos on YouTube which have done it but do not have a description of motor & power supply used.

    The following is a shop based in my area(Link below)

    Bombay Electronics - DC Motors

    Please suggest motor which would suit best for my need from the above website,also provide the corresponding power supply Voltage & Amperage value I should use with motor on full load.

    Awaiting for your advice!

    Thanks in advance!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jw0752

    Thank you John for your detailed answer!

    I was thinking of making drill with USB power supply(5v)

    There are videos on YouTube which have done it but do not have a description of motor & power supply used.

    The following is a shop based in my area(Link below)

    Bombay Electronics - DC Motors

    Please suggest motor which would suit best for my need from the above website,also provide the corresponding power supply Voltage & Amperage value I should use with motor on full load.

    Awaiting for your advice!

    Thanks in advance!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 10 years ago in reply to e14 Contributor

    Hi Apoorva,

     

    The only size drills that could be successfully utilized with such a small motor and low power power supply would be 1.5 mm or less in diameter. It would also be a challenge to mount the drill concentrically on the motor shaft. Even mounting a small chuck if available would be a challenge. If you were to us a USB power supply choosing the one with the most amperage rating would be your best bet. 2 amps at 5 volts would give you about 10 watts of power available.

     

    John