Community Feedback
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Community Feedback
  • More
  • Cancel
Community Feedback
Forum Basic Electronic Queries
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Feedback to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 3 answers
  • Subscribers 7 subscribers
  • Views 1569 views
  • Users 0 members are here
Related

Basic Electronic Queries

e14 Contributor
e14 Contributor over 10 years ago

Hi,I had following queries :

1.Are 1602 and 16*2 just different names for same LCD module?

2.How  to identify whether the cheap LCD modules has HD44780 controller board inbuilt?

3. While operating DC brushed motor if it is specified 5v-9v ,what is safe operational voltage? 4. While operating DC brushed motor how to calculate amperage rating to prevent frying out power supply?

5.Which are best type of DC motor for attaching drill bits?

Awaiting for reply! Thank you!

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago +3 suggested
    Just to add some more useful info on the LCD's - you can often buy them with an i2c backpack which can simplify their usage and reduce the amount of wires to connect to them considerably, by buying one…
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Just to add some more useful info on the LCD's - you can often buy them with an i2c backpack which can simplify their usage and reduce the amount of wires to connect to them considerably, by buying one with a backpack you also need not worry about the controller chip as the datasheet will list all of the commands you need to communicate with it through i2c.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 10 years ago in reply to e14 Contributor

    by buying one with a backpack you also need not worry about the controller chip as the datasheet will list all of the commands you need to communicate with it through i2c.

    While I agree that the datasheet will give you the commands, it is based on the underlying controller chipset.

     

     

    For clarification.

    The I2C "backpack" is simply an I2C to 8 bit expander.

    They are available already attached or seperately (for a couple of $) to add to most LCD's that use parallel interface. (ie have the 14 or 16 pins)

    It simply provides a piece of hardware that converts what you send via the I2C interface into the multiple pins on the LCD.

    They also have one big advantage in that they drive the Backlight without an external transistor, since these normally draw more current than a pin on the Arduino can handle.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 10 years ago in reply to e14 Contributor

    by buying one with a backpack you also need not worry about the controller chip as the datasheet will list all of the commands you need to communicate with it through i2c.

    While I agree that the datasheet will give you the commands, it is based on the underlying controller chipset.

     

     

    For clarification.

    The I2C "backpack" is simply an I2C to 8 bit expander.

    They are available already attached or seperately (for a couple of $) to add to most LCD's that use parallel interface. (ie have the 14 or 16 pins)

    It simply provides a piece of hardware that converts what you send via the I2C interface into the multiple pins on the LCD.

    They also have one big advantage in that they drive the Backlight without an external transistor, since these normally draw more current than a pin on the Arduino can handle.

     

    Mark