Community Feedback
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Community Feedback
  • More
  • Cancel
Community Feedback
Forum Is the timer of an arduino accurate enough to build a clock or do I need a RTC?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Feedback to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 8 subscribers
  • Views 2896 views
  • Users 0 members are here
  • tft display
  • arduino time
  • arduino
Related

Is the timer of an arduino accurate enough to build a clock or do I need a RTC?

simon.ganne
simon.ganne over 8 years ago

Is the timer of an arduino accurate enough to build a clock or do I need a RTC? I have some problems with the precision of my clock. I use a TFT display to show the date and the time, it works just fine but the clock is running too slow. has anyone a solution?  I'm going to use this in a project, the code is not complete yet but I have to get this part right first. Here is my code:

#include <Adafruit_GFX.h>
#include <MCUFRIEND_kbv.h>                                // bibliotheek voor het communiceren met het diplay 
#include "DHT.h"
#include <stdio.h>


MCUFRIEND_kbv tft;                                        // maak een display aan
DHT dht;


#if defined(__SAM3X8E__)
#undef __FlashStringHelper::F(string_literal)
#define F(string_literal) string_literal
#endif


#define BLACK       0x0000      /*   0,   0,   0 */
#define WHITE       0xFFFF      /* 255, 255, 255 */


uint8_t hh, mm, ss;
int date_month, date_day, date_year;
String date_month_string, date_day_string, date_year_string;
unsigned long time_val, old_time_val, old_time_val_1;


int text_size = 3;
int time_cursor_x = 10;
int time_cursor_y = 110;


uint8_t conv2d(const char* p)
{
  uint8_t v = 0;
  if ('0' <= *p && *p <= '9') v = *p - '0';
  return 10 * v + *++p - '0';
}
void setup() {
  // put your setup code here, to run once:
  Serial.begin(9600);                               // begin de seriële monitor
  while (!Serial) ;                                 // wacht tot deze is opgestard
  String date_string = __DATE__;


  tft.reset();                                      // reset het tft display
  tft.begin(0x7783);                                // begin de communicatie met het display met adres 0x7783
  tft.setRotation(1);                               // roteer het display zodat het in landscape modus staat
  tft.fillScreen(BLACK);


  hh = conv2d(__TIME__);
  mm = conv2d(__TIME__ + 3);
  ss = conv2d(__TIME__ + 6);
  date_month_string = date_string.substring(0, 3);
  date_day_string = date_string.substring(4, 6);
  date_year_string = date_string.substring(7, 11);


  date_year = date_year_string.toInt();
  date_day = date_day_string.toInt();
  date_month = month_string_to_int(date_month_string);
  OCR0A = 0xAF;
  TIMSK0 |= _BV(OCIE0A);
}
void loop() {
  // put your main code here, to run repeatedly:
  text_size = 3;
  time_cursor_x = 10;
  time_cursor_y = 110;
}
SIGNAL(TIMER0_COMPA_vect){
  time_val = millis();
  if ((time_val - old_time_val) >= 1000) {
    if (++ss > 59) {
      ss = 0;
      mm++;
      if (mm > 59) {
        mm = 0;
        hh++;
        if (hh > 23) {
          hh = 0;
          date_day++;
          if (date_day == 31 && (date_month == 1 || date_month == 3 || date_month == 5 || date_month == 7 || date_month == 8 || date_month == 10 || date_month == 12)) {
            date_day = 0;
            date_month++;
            if (date_month > 11) {
              date_month = 1;
              date_year++;
            }
          }
          if (date_day == 30 && (date_month == 4 || date_month == 6 || date_month == 9 || date_month == 11)) {
            date_day = 0;
            date_month++;
          }
          if (date_day == 28 && date_month == 2 && (date_year % 4) != 0) {
            date_day = 0;
            date_month++;
          }
          if (date_day == 29 && date_month == 2 && (date_year % 4) == 0) {
            date_day = 0;
            date_month++;
          }
        }
      }
    }
    tft.setTextColor(WHITE);
    tft.setTextSize(text_size);
    char buf[8];
    char buf_2[12];
    sprintf(buf_2, "%02i/%02i/%04i", date_day, date_month, date_year);
    sprintf(buf, "%02d:%02d:%02d", hh, mm, ss);
    tft.setCursor(time_cursor_x, time_cursor_y);
    tft.fillRect(time_cursor_x, time_cursor_y, 50 * text_size, 7 * text_size , BLACK);
    tft.print(buf);
    tft.setCursor(time_cursor_x, time_cursor_y + 8 * text_size);
    tft.fillRect(time_cursor_x, time_cursor_y + 8 * text_size, 60 * text_size, 7 * text_size , BLACK);
    tft.print(buf_2);
    Serial.println("tijd weergegeven");
    old_time_val = time_val;
  }
}
int month_string_to_int(String date_month_string) {
  if (date_month_string == "Jan")return 1;
  if (date_month_string == "Feb")return 2;
  if (date_month_string == "Mar") return 3;
  if (date_month_string == "Apr") return 4;
  if (date_month_string == "May") return 5;
  if (date_month_string == "Jun") return 6;
  if (date_month_string == "Jul") return 7;
  if (date_month_string == "Aug") return 8;
  if (date_month_string == "Sep") return 9;
  if (date_month_string == "Oct") return 10;
  if (date_month_string == "Nov") return 11;
  if (date_month_string == "Dec") return 12;
}

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +9 verified
    Hi Simon, The arduino is as accurate as a typical home clock, because it uses a crystal oscillator. However, you're using the millis() function and although there is a risk of an assumption that this provides…
  • ntewinkel
    ntewinkel over 8 years ago +6 suggested
    Hi Simon, Maybe try the Time library? It seems to take care of most of the details for you. https://playground.arduino.cc/Code/Time Cheers, -Nico
  • beacon_dave
    beacon_dave over 8 years ago +4 suggested
    You don't say how accurate the clock needs to be an or the intended operating conditions. However there is also the internal RC oscillator, which can be calibrated for improved accuracy: http://www.atmel…
Parents
  • beacon_dave
    0 beacon_dave over 8 years ago

    You don't say how accurate the clock needs to be an or the intended operating conditions. However there is also the internal RC oscillator, which can be calibrated for improved accuracy:

    http://www.atmel.com/Images/Atmel-2555-Internal-RC-Oscillator-Calibration-for-tinyAVR-and-megaAVR-Devices_ApplicationNot…

     

    This would have to be calibrated on a per microcontroller device basis, so not so convenient for large quantities. It is also susceptible to voltage and temperature so you probably want to calibrate it in typical usage conditions for best results.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • beacon_dave
    0 beacon_dave over 8 years ago

    You don't say how accurate the clock needs to be an or the intended operating conditions. However there is also the internal RC oscillator, which can be calibrated for improved accuracy:

    http://www.atmel.com/Images/Atmel-2555-Internal-RC-Oscillator-Calibration-for-tinyAVR-and-megaAVR-Devices_ApplicationNot…

     

    This would have to be calibrated on a per microcontroller device basis, so not so convenient for large quantities. It is also susceptible to voltage and temperature so you probably want to calibrate it in typical usage conditions for best results.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer