Community Feedback
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Community Feedback
  • More
  • Cancel
Community Feedback
Forum HP Compaq G750 USB Conversion
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Feedback to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 6 subscribers
  • Views 1577 views
  • Users 0 members are here
  • max232
  • hp
  • pocket_pc
  • rs232
  • keyboard input
  • arduno
Related

HP Compaq G750 USB Conversion

rtm516
rtm516 over 8 years ago

Hello,

I need help working out how to convert the HP Compaq G750 to USB using an Arduino pro micro. So far I have worked out that it uses RS232 so hooked it up using a MAX232EPE to the Arduino and loading the attached sketch onto it. I now get feedback over serial but I don't understand how to parse it as I can't find any info on this online and don't have any more advanced tools like an oscilloscope to make sure I'm using the correct baud rate. I have attached some data I have pulled with various actions. If needed I can provide a fritzing sketch with my wiring layout but it is based on https://imgur.com/vxgZs  without the 10uF capacitor or that trace. I have also attached a few pictures of the inside of the connector and its wiring. (I hooked it up with 3.3v)

 

Any help would be appreciated, Thanks.

Attachments:
iPAQ_Keyboard.ino.txt.zip
Keyboard data.txt.zip
image
image
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +2 suggested
    You have a variable length of bits, sometimes 21 bits, and sometimes 23 bits and sometimes 24 bits. I can't see a pattern, but was just wondering, why not pattern match on all these bits, it wouldn't take…
Parents
  • shabaz
    0 shabaz over 8 years ago

    You have a variable length of bits, sometimes 21 bits, and sometimes 23 bits and sometimes 24 bits.

    I can't see a pattern, but was just wondering, why not pattern match on all these bits, it wouldn't take a lot of flash memory.

    You'd need to compare the input bits with all the patterns stored in memory, until you find one that matches, or (easier) that has the longest match.

    It is not ideal, but in theory I can't see why that wouldn't work.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rtm516
    0 rtm516 over 8 years ago in reply to shabaz

    Do you mean go through each key and save the data in a big array, then just check the received data on that array and then send the correct key?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rtm516
    0 rtm516 over 8 years ago in reply to shabaz

    Do you mean go through each key and save the data in a big array, then just check the received data on that array and then send the correct key?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 8 years ago in reply to rtm516

    Yes, that would work.