Community Feedback
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Community Feedback
  • More
  • Cancel
Community Feedback
Forum Logic game
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Feedback to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 11 subscribers
  • Views 1589 views
  • Users 0 members are here
Related

Logic game

waterfield
waterfield over 9 years ago

the heated discussion  about the bus bars was fun. So that everyone is happy why not have the magnets on the end of the wire and small steel strips around the board, they could then be used as bus bars or alternatively for storing/hanging the leads when not in use.

good luck with the build

paul

  • Sign in to reply
  • Cancel

Top Replies

  • tocsoft
    tocsoft over 9 years ago +1
    Another option would have the connectors be stackable, you can then simplify the board but then increment the difficulty later to require the stack/split connections. Something like this very (very) rough…
  • gordiegii
    gordiegii over 9 years ago in reply to makerkaren +1
    In my experience logic gets boring fast if you can't advance the complexity of circuits. Fortunately you don't need buss bars to have signals go to multiple inputs. All you need is two connectors at each…
Parents
  • c.creehan
    c.creehan over 9 years ago

    I agree that the prime directive here should be to make an educational tool, but at the same time I feel like could be "too simple" with the limitations of not including bus bars.

     

    In my mind there are 2 possible solutions:

         1. Include them as an optional extra or "expansion pack"

         2. Find a way to do it without adding too much complexity. ie stacking connectors, mounted.

     

    Either way, I would argue that the addition of further complexity or expandablility would broaden your market. This could be a great teaching tool but why stop there? It could also be a great puzzle game for adults. There's no reason it can't appeal to both markets.

     

     

    Secondly, love the magnetic connectors. Found these online Dia 3/8x1/8" Countersunk Magnets | CMS Magnetics  The look like they have potential to work well.
    Like if you had a plastic "cap" that housed a wire with a ring terminal and a screw went through this magnet into the plastic to hold it all together.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • c.creehan
    c.creehan over 9 years ago

    I agree that the prime directive here should be to make an educational tool, but at the same time I feel like could be "too simple" with the limitations of not including bus bars.

     

    In my mind there are 2 possible solutions:

         1. Include them as an optional extra or "expansion pack"

         2. Find a way to do it without adding too much complexity. ie stacking connectors, mounted.

     

    Either way, I would argue that the addition of further complexity or expandablility would broaden your market. This could be a great teaching tool but why stop there? It could also be a great puzzle game for adults. There's no reason it can't appeal to both markets.

     

     

    Secondly, love the magnetic connectors. Found these online Dia 3/8x1/8" Countersunk Magnets | CMS Magnetics  The look like they have potential to work well.
    Like if you had a plastic "cap" that housed a wire with a ring terminal and a screw went through this magnet into the plastic to hold it all together.