Community Feedback
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Community Feedback
  • More
  • Cancel
Community Feedback
Forum Trying to get USB to front NES ports.
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Feedback to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 8 subscribers
  • Views 1581 views
  • Users 0 members are here
Related

Trying to get USB to front NES ports.

darkloud
darkloud over 9 years ago

Hey guys! First post here! I am trying to get 2 standard USB ports to the front of a NES case. As in, I do not want to use the controller ports, but rather mount a single USB port per player slot. As I do not have a 3d printer, I am kind of at a loss at how to mount the ports to the front? Once the controller ports are removed you are left with a large gaping hole.

 

What do you guys think they best thing would be to do to get USB ports mounted to the front?

 

Also do any of you know where to purchase the USB connectors? As in just the metal piece that connects the devices together? I figure it would much more easier to make something to mount with that rather than a preassembled USB cable...

 

Best regards!

  • Sign in to reply
  • Cancel

Top Replies

  • aoshiryunda
    aoshiryunda over 9 years ago +1
    I'm making a raspberry pi conversion on my NES. I have a 3d printer, so if you don't end up buying one, let me know in message and I can design one up in Fusion 360 and help you out. I just finished a…
Parents
  • shabaz
    shabaz over 9 years ago

    Hi Warren,

     

    You mean to just physically use the USB connector although it will not be using USB communications (i.e. normal USB devices will not function if plugged in)?

    If so, google for 'chassis mount USB connector', you'll find quite a few different varieties, some of which just require a large circular hole which is easy to do with a drill, although it will need to be a large diameter drill - a step drill bit could be used, or (cheaper) just drill lots of small holes in a circle, then use a half-round file).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 9 years ago

    Hi Warren,

     

    You mean to just physically use the USB connector although it will not be using USB communications (i.e. normal USB devices will not function if plugged in)?

    If so, google for 'chassis mount USB connector', you'll find quite a few different varieties, some of which just require a large circular hole which is easy to do with a drill, although it will need to be a large diameter drill - a step drill bit could be used, or (cheaper) just drill lots of small holes in a circle, then use a half-round file).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • darkloud
    darkloud over 9 years ago in reply to shabaz

    Thanks for the advice! Not exactly what I meant however I googled the query you suggested and it did yield some connectors which may work for my needs! Thank you so much!  I also found a Monoprice Mini 3D printer on craigslist for 100 bucks so I am trying to get that and then most of these fabrication problems will be a thing of the past hopefully.