element14's The Ben Heck Show
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • More
  • Cancel
element14's The Ben Heck Show
Documents Ben Heck's Essentials Series: Wireless Communications -- Episode 267
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join element14's The Ben Heck Show to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: randogless
  • Date Created: 8 Dec 2016 10:46 PM Date Created
  • Last Updated Last Updated: 2 Dec 2016 8:24 AM
  • Views 1728 views
  • Likes 2 likes
  • Comments 4 comments
Related
Recommended

Ben Heck's Essentials Series: Wireless Communications -- Episode 267

image

element14's The Ben Heck Show

Join the Ben Heck team every week for amazing hacks! Watch them build and mod community-inspired projects using electronics!

Back to The Ben Heck Show homepage image

Connect with TBHS
Featured Bonus Content
See All Episodes

 

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

To untangle Karen from her mess of wires the team discusses everything related to wireless communication! Learn the difference between ELF, SLF, ULF, VLF, LF, MF, HF UHF, and THF frequency bands and different technologies for electronics communication such as WIFI, xBee, Bluetooth, RFID, NFC, and mobile networks.

 

Ben goes over commonly used radio frequency bands. ELF, extremely low frequency (3-30Hz range), is generally used for long range communication like submarine use and maritime use.  SLF, super low frequency (30-300Hz range), is still mostly maritime use. VLF, Very Low Frequency (3kHz-30kHz range), is still used for mostly radio navigation and maritime military use. LF, Low Frequency (30kHz-300kHz range), is still used for a lot of radio navigation but it’s also used for amateur radio and universal clock signals. MF, Medium Frequency (300kHz-3MHz range), is used for AM radio. HF, High Frequency (3MHz-30MHz range), is used for short wave radio, CB radio, RFID radar, and more amateur radio. VHF, Very High Frequency (30MHz -300MHz range), is used for FM broadcasts and TV broadcasts. UHF, 300MHz-3000 MHz, is used for TV, cell phones, and other consumer devices. SHF, Super High Frequency (3GHz-30GHz range), is used for WIFI and cellular technology as well as microwave transmitters. EHF, Extremely High Frequency (30GHz-300GHz range) is used for radio astronomy and the millimeter wave scanner used for airport security.  THF, Tremendously High Frequency (300GHz-3000GHz range), is used for crazy experimental stuff like particle physics, medical imaging, atomic blasters, and things of that elk.

 

The 2.4 GHz /5 GHz wireless range is usually expressed when referring to the 802.11 (a, b, g, and n) wireless standards. 2.4 GHz is a popular range for products with their own proprietary protocols.

 

2.4 GHz is the most common protocol with the XBee signal.  XBee signals are a little slower than Bluetooth but they have a longer range. XBee signals are a good choice if you have to do point to point data transfers.

 

Bluetooth runs in the 2.4 GHz range as well.  The difference between Bluetooth and Wifi is the range is shorter and the bandwidth is much less. Bluetooth is best for connecting peripherals to a nearby host device. Bluetooth allows you to pair enabled devices to multiple systems where as WiFi is more of an ad hoc network.  Ben and Felix examine various Bluetooth enabled devices. The advantage of Bluetooth is that it is a ubiquitous standard and has low power consumption.  However, it has a shorter range of transfer and lacks support for large data transfers making it ideal for audio but not video.

 

RFID, radio frequency identification, technology uses two parts, a tag and a reader. The tag has a number and the reader interprets that. There are two different types of tags, Active Tags and Passive Tags. An Active Tag has a power source in it so it can emit the signal and a passive tag takes the signal, use the wireless transmitted from the reader to power itself to spit back the signal. Some have a small amount of RAM so they can send back more than just a number or a larger number. RFID technology allows an administrator to grant or restrict access remotely.  Unlike using physical keys, you can restrict access to a facility without having to change the locks on the building.

 

NFC, Near-Field Communication, is like RFID, but smaller distances and actively controlled by a phone instead of just a static tag.  Apple Pay is an example of this. The shorter range makes it more secure because people cannot intercept the signals. RFID uses a passive tag with a number on it that can be read whereas NFC can be two way communication and the tags are active so it can change the information and number its sending. An NFC cell phone can work as the reader or the tag and go both ways.

 

Finally, they discuss cellular protocols.  1G, 2G or Edge Network, 3G, and 4G LTE are discussed.   Multi-band GSM phones can work anywhere, including other countries.  Multiple bands increase the chance a carrier is compatible.

  • episode 267
  • hack
  • episode 267: ben heck's essentials series: wireless com
  • heck
  • ben
  • tbhs_ep
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +1
    I have an interesting wireless project for you Ben. I have been thinking about a wireless repeater station for people mapping caves. Basically, you need to set up a repeater as you go deeper into the cave…
  • beacon_dave
    beacon_dave over 9 years ago in reply to DAB +1
    Doesn't ZigBee / DigiMesh pretty much give you that sort of mesh functionality out of the box ? https://www.digi.com/pdf/wp_zigbeevsdigimesh.pdf
  • charlie68
    charlie68 over 9 years ago +1
    Hey Team, so a wireless project ... The problem: Lots of people have leisure vehicles, motor homes, boats, caravans etc, mostly not stored at home. i have a sailboat on a river. and sit at home worrying…
  • charlie68
    charlie68 over 9 years ago

    Hey Team,

     

    so a wireless project ...

     

    The problem:

    Lots of people have leisure vehicles, motor homes, boats, caravans etc, mostly not stored at home. i have a sailboat on a river. and sit at home worrying if it has sunk or not...

     

    The suggestion:

     

    How about a remote monitoring system? I would love to use my phone to find out if my boat was o.k. e.g. battery voltages are healthy, gps position of the boat (has the anchor dragged?), is it sinking? (is there water in the bilges), what's the temperature and humidity on the boat? Maybe send a photo of lovely blue skies to encourage me to go sailing : )

     

    I would guess this is perfect for your 3G module and a micro controller. The device would have to be low power, wake up say every 30 mins, report and go back to sleep (so as not to kill the boats solar maintained 125AH 12V lead acid battery).

     

    I guess that means it would need to send data "to the cloud man" for viewing on demand. it would be great to get text alerts "help i'm sinking!" or "call the cops someones stealing me!" or "arrrh i'm dying! ..." (well the battery is dying...).

     

    it might need:

    *: a nice case to keep some sensors & electronics tidy with status lights & a control panel for when you are on the boat.

    * Maybe a custom water sensor design/enclosure.

    * Some cloud/web or maybe phone software ....

     

    Feels like a two episode 3 person team project to me : )

     

    Thanks and I hope you like the idea - Happy Christmas to all!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 9 years ago in reply to DAB

    Doesn't ZigBee / DigiMesh pretty much give you that sort of mesh functionality out of the box ?

    https://www.digi.com/pdf/wp_zigbeevsdigimesh.pdf

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    I have an interesting wireless project for you Ben.

     

    I have been thinking about a wireless repeater station for people mapping caves.

    Basically, you need to set up a repeater as you go deeper into the cave so that you can maintain a connection to devices outside the cave.

     

    It would be a really useful capability and you could also use it in search and rescue operations to maintain contact inside large buildings or areas where direct line of sight is compromised.

     

    Just a thought.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Great Episode and review of the RF spectrum.

     

    I had not been keeping up with the RF allocation, so I found the information very useful.

     

    DAB