element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum 1n4148
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 143 subscribers
  • Views 2068 views
  • Users 0 members are here
Related

1n4148

alisabiee
alisabiee over 6 years ago

What does 1n4148 do in these circuits?imageimage

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 6 years ago +5
    1st schema: the 1N4148 is a temperature sensor. The forward voltage is dependent on temperature. source: Vishay datasheet @farnell . The voltage at the R1-D1 node will be will be around 0.6 - 0.7 V, but…
  • Jan Cumps
    Jan Cumps over 6 years ago +4
    Second circuit I'm going to guess that the reverse breakdown voltage of the transistor basis-emitter is less than what can occur in this circuit, with that output circuit keeping the mid-point a short…
  • beacon_dave
    beacon_dave over 6 years ago in reply to Jan Cumps +2
    Its function is also described in the original blog here: Simple temperature sensor diode 1N4148 https://www.eleccircuit.com/measurements-temperature-by-diode-1n4148/
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to beacon_dave +1
    few, I'm not far off. now circuit 2. Let's see how I passed or failed. I think that the one of the transistors can go up to almost 12V reverse bias (mid point 12 V, Vosc 0) and the other one 24 V reverse…
  • Jan Cumps
    Jan Cumps over 6 years ago

    1st schema: the 1N4148 is a temperature sensor.

    The forward voltage is dependent on temperature.

     

     

    image

    source: Vishay datasheet @farnell.

     

    The voltage at the R1-D1 node will be will be around 0.6 - 0.7 V, but varies.

    The current through the diode will be (15 V - 0.6 V) / 15 K = almost 1  mA (953 µA).

    So it will follow the second-lowest trace and have 0.6 V at 40°C.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago

    Second circuit I'm going to guess that the reverse breakdown voltage of the transistor basis-emitter is less than what can occur in this circuit, with that output circuit keeping the mid-point a short time at +12 at falling edge and -12V at rising edge.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 6 years ago in reply to Jan Cumps

    Its function is also described in the original blog here:

     

    Simple temperature sensor diode 1N4148

    https://www.eleccircuit.com/measurements-temperature-by-diode-1n4148/

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to beacon_dave

    few, I'm not far off.

     

    now circuit 2. Let's see how I passed or failed. I think that the one of the transistors can go up to almost 12V reverse bias (mid point 12 V, Vosc 0) and the other one 24 V reverse (mid point -12V; Vosc +12V).

    The transistors can typically have 5 - 6 V.