element14 presents
  • Challenges & Projects
  • More
element14 presents
element14 presents Forum Making a Soundboard with a Raspberry Pi
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • +1 person also asked this people also asked this
  • Replies 9 replies
  • Subscribers 141 subscribers
  • Views 4997 views
  • Users 0 members are here
  • python
  • help
  • pi
  • projects
  • raspberry pi
  • Python script
  • help!
Related

Making a Soundboard with a Raspberry Pi

raf1983
raf1983 over 2 years ago

Hi All,

Im new to programing and to python (so please excuse and mistakes).

So im trying to make a soundboard for an old Raspberry to play Train staion sounds for my nephew.

This is the list of equiptment im using.
Ras Pi 2 B+
16GB sd card
USB NumberPad (Logik NO:LKBNP10)

I was hoping to use the onboard headphone jack but i have a UBS sound card if i need.

Have install (i think) all the softwear i need as i can play sound with ether “cvlc” or a sound test python script.

i have used “ChatGPT” to make a script but nomatter what i try i cant get the sctript for the sound board to work.

So this is what i want to do as a compleat project.
1: I would like the pi to play a sound once the pi is booted and the script is ready to use.
2: the script to run once the pi is booted.
3: A SoundBoard script
4: Use the keypad numbers 0-9 to play diffrent mp3 files (i have made 10 files to use)
5: As there are 18 buttons on the keypad (not including the NUM LOCK key) i would like to use the + and - to controle volume and the * key to shutdown the pi.

Hopfully these are possible.

Here is the script i have so far,

import pygame
import os
from evdev import InputDevice, ecodes

def play_sound(sound_path):
pygame.mixer.init()
sound = pygame.mixer.Sound(sound_path)
sound.play()
pygame.time.delay(int(sound.get_length() * 1000)) # Wait for sound to finish

def find_number_pad():
devices = [fn for fn in os.listdir(‘/dev/input/’) if fn.startswith(‘event’)]
for device_fn in devices:
device_path = f’/dev/input/{device_fn}’
try:
device = InputDevice(device_path)
print(f"Detected device: {device.name}")
if “0410:0001” in device.name:
return device
except FileNotFoundError:
pass
return None

def main():
sound_folder = “/home/rich/sounds” # Replace with the actual path to your so>

key_to_sound = {
    ecodes.KEY_1: "11.mp3",
    ecodes.KEY_2: "12.mp3",
    ecodes.KEY_3: "13.mp3",
    ecodes.KEY_4: "14.mp3",
    ecodes.KEY_5: "15.mp3",
    ecodes.KEY_6: "16.mp3",
    ecodes.KEY_7: "17.mp3",
    ecodes.KEY_8: "18.mp3",
    ecodes.KEY_9: "19.mp3",
    ecodes.KEY_0: "20.mp3"
}

number_pad = find_number_pad()
if not number_pad:
print(“USB number pad not found. Exiting.”)
return

pygame.init()

try:
    while True:
        for event in number_pad.read_loop():
            print(f"Event: {event}")
            if event.type == ecodes.EV_KEY and event.value == 1:
                key = event.code
                if key in key_to_sound:
                    sound_path = os.path.join(sound_folder, key_to_sound[key])
                    print(f"Playing sound: {sound_path}")
                    play_sound(sound_path)

except KeyboardInterrupt:
    pygame.quit()

if name == “main”:
main()

when i run the script and press a number on the key pad this is what i get

pygame 2.5.2 (SDL 2.0.14, Python 3.9.2)
Hello from the pygame community. Contribute - pygame wiki
Detected device: vc4-hdmi
Detected device: HID 0410:0001

and the script just hangs.

0410:0001 is the device name of the keypad and i have set the headphone jack as the default in raspi config.

If anyone could help it would make my nephew so happy as this is a supprise for him.

Im more them happy to do a clean install of raspian lite if this will help.

Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 2 years ago +1
    Hi, I dont currently have time to check your script others might help you out, in the meantime, an alternative approach possibly worth reading to rule in or out, could be to use a Pi Pico. An example…
  • fmilburn
    fmilburn over 2 years ago +1
    I haven't programmed in Python in a while but I wrote a program using pygame on a laptop a few years back that can be found here . My program used wav files rather than MP3. Notice how simple it is - I…
  • beacon_dave
    beacon_dave over 2 years ago +1
    raf1983 said: Detected device: HID 0410:0001 That print output should give you a clue where to start. The next step after that is to test if "0410:0001" is in device.name, so you could add a print…
  • robogary
    robogary over 2 years ago +1
    https://magpi.raspberrypi.com/books/handbook-2023 another resource
Parents
  • robogary
    0 robogary over 2 years ago

    https://magpi.raspberrypi.com/books/handbook-2023   another resource 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • robogary
    0 robogary over 2 years ago

    https://magpi.raspberrypi.com/books/handbook-2023   another resource